Variable Load Hookup Guide - Revised

≡ Pages
Contributors: SFUptownMaker

Changing the Firmware

All of the firmware is available on the GitHub page for the product. You can customize the firmware as you need using the bootloader on the board, without having to use a programming cable, so long as your board has the most updated firmware. Boards shipped prior to 24 May 2018 do not have a bootloader on them.

PSoC Creator

Download and unzip the files from the GitHub repository for the Variable Load board.

Open the Variable_Load.cyprj project file in PSoC Creator. Under the build configuration, set it to Release mode.

Select Release Mode

In the menu bar, select Build > Build All Projects to generate the files for the project. The one that we are interested in is the application file for the bootloader (Variable_Load.cyacd) which will be used later.

Build All Projects

Entering Bootloader Mode

To place the board in bootloader mode, open a console connected to the board and type "B" and hit Enter. The console will lose its connection and the board will reenumerate with a different port number. You can now bootload the board.

Using the Bootloader Host Application

To open the bootloader host application, open the "Tools" menu in PSoC Creator and select "Bootloader Host...".

Where to find the bootloader host menu item in creator

This window will appear. Select the new COM port number for your board in the list.

The bootloader host application window

Baud rate, data bits, stop bits and parity can all be left as-is. So can "Active application", and the "Security key" box can be left unchecked. Click the "..." button next to the file to bring up the file selection dialog.

The application file for the bootloader is of type "*.cyacd" and it can be found in the firmware directory under ".../CortexM3/ARM_GCC_541/Release", assuming you are using PSoC Creator 4.2 with a build configuration set in Release mode.

The path to the bootloader app file

The *.cyacd file will automatically be generated whenever the project is built. Note that using the "Program" button in the main PSoC Creator menu bar does not work for bootloaded projects!

The last step in the bootloading process is to click the "Program" button in the button bar at the top of the Bootloader Host window. You should see messages indicating a successful programming scroll past in the text window at the bottom of the window.

Where to find the program button