Tsunami Super WAV Trigger Hookup Guide

≡ Pages
Contributors: santaimpersonator

Prepare the μSD Card

Format the µSD Card

Note: For the best results, we recommend Class 10 SD cards with a FAT16 or FAT32 file system format and a 32kB file allocation size. We recommend avoiding:

  • The 1GB SparkX SD Card, from our catalog, since it isn't a Class 10 card and can lead to reliability issues.
  • SD Cards with a capacity larger than 32GB, since it can be difficult to convert them to the FAT16 or FAT32 file system format with a 32kB file allocation size.

For more information on compatible SD cards, please check out the Robertsonics website:

The µSD card is an integral part of the Qwiic Tsunami's operation. In order for the µSD card to be compatible with the Qwiic Tsunami:

  • A FAT16 or FAT32 file system must be used
  • The file allocation size must be 32 kilobytes

For a brand new card, formatting may not be necessary. However, if users experience the Qwiic Tsunami missing commands, making occasional strange buzzing sounds, or sometimes crashing, then the file allocation size may be incorrect. The Quick Format option in the Windows operating system is the usually the simplest method to properly format the µSD card.

Formatting an SD card with a Window OS
The format settings for a µSD card with a Windows operating system. (Click to enlarge)

µSD Card Contents

The contents of the µSD card are the key to how the Qwiic Tsunami operates. There are two types of files that the firmware on the Qwiic Tsunami will utilize: audio *.wav files and a tsunami.ini initialization file. The firmware on the Qwiic Tsunami, by default, is configured to operate in the following manner:

  1. Default firmware operation (filenames matching the trigger inputs, will output on the first audio output channel 1L).
  2. If there is a tsunami.ini file on the µSD card on reset, the Qwiic Tsunami will operate on its configuration content.
  3. Any additional changes via I2C or serial commands then take precedence over the initialization file.

Audio Files

The Qwiic Tsunami is designed to playback *.wav audio files from the µSD card. However, the *wav files must be compatible with the firmware on the Qwiic Tsunami.

  • The audio format of *.wav files must be compatible with the firmware on the Qwiic Tsunami.
    • By default, the Qwiic Tsunami is factory programmed with the mono audio firmware and will only work with *.wav files in mono audio format.
  • The filenames if the *wav files must follow the naming convention utilized by the firmware for the Qwiic Tsunami to trigger the audio playback.
Audio File Format

The Qwiic Tsunami plays *.wav files recorded at 16-bit resolution, with a 44.1kHz sampling rate. Different firmware images allow for the playback of stereo or mono files. The Qwiic Tsunami also requires that the files not contain any additional header information. Some audio recording programs, such as Pro Tools, write additional information at the start of the file. An easy way to remove the unnecessary header information is to utilize Audacity. Users can use this software to export a file as WAV (Microsoft) signed 16-bit PCM and clear out the metadata containing the header infromation (i.e. title, artist, genre, etc.).

The following video gives a brief demonstration of the Audacity export process.

Exporting from Audacity to Tsunami. (Click to enlarge)

Note: For users curious about the header contents, Rail John Rogut has written the Header Investigator application, which can display Pro Tools region information and BWF time stamps. This extra data might be meaningful to DAW applications, but Tsunami doesn't use the information.
Naming Convention

The filenames contain the trigger input mapping for the Qwiic Tsunami. Each file should start with a three-digit number, which will assign it to a corresponding trigger input.

example trigger map

Example of a filename trigger mapping. (Click to enlarge)

In the example above, the firmware on the Qwiic Tsunami will correspond the filenames of the 16 files numbered 001 to 016 to each of the trigger inputs by default. The triggered *.wav files would be output on the first audio channel (1L).

Initialization File

Note: When creating an intialization *.ini file with the configuration tool, users should make sure to select the proper settings for the firmware on the Qwiic Tsunami. By default, the Qwiic Tsunami factory programmed firmware is configured for the mono setting and the configuration tool settings should match the image below:

example settings
Example default settings in the configuration tool. (Click to enlarge)

Below is a comparison of the configuration tool appearance between the mono and stereo settings. Users will notice that some of the audio channel output options are greyed-out in the stereo setting.

stereo setting
The stereo setting option for the configuration tool. (Click to enlarge)
mono setting
The mono setting option for the configuration tool. (Click to enlarge)

There is also an initialization file, tsunami.ini. The Qwiic Tsunami reads this file when it starts, to gather more details about how it should configure the trigger inputs. The *.ini files can be generated and edited using the Tsunami Configurator application. The files contain readable ASCII text, which can be created or edited with a text editor.

configuration tool

Tsunami configuration tool. (Click to enlarge)

More information about the configuration tool can be found in the Tsunami user guide under "The Init file and the Robertsonics Configurator Utility app".

Firmware

The firmware on the Qwiic Tsunami, by default, is configured to operate in the following manner:

  1. Default firmware operation (filenames matching the trigger inputs, will output on the first audio output channel 1L).
  2. If there is a tsunami.ini file on the µSD card on reset, the Qwiic Tsunami will operate on its configuration content.
  3. Any additional changes via I2C or serial commands then take precedence over the initialization file.

Updating the Firmware

When necessary, users can easily update the firmware by saving the file to the µSD card. The latest firmware for the Qwiic Tsunami can be found on Robertsonics website. The file name needs to be changed to tsunami.hex for the bootloader to upload the new firmware. Once the files is saved onto the µSD card, users need to follow the following procedures to update the firmware on the board:

  1. Hold the USER button down
  2. Insert SD card with new firmware tsunamix.hex file (can have normal operation *.wav and *.ini files)
  3. Press RESET button
  4. Wait for successful firmware update status indicator before releasing the USER button
    • When the status LED is a solid green, the firmware update is complete.

Example Files

For the examples in the following section, users will need to prepare their card with the demonstration files we provide.

  1. Download the example files using the link below.
  2. Unzip the folder and put the files on the root directory of the card.
  3. Verify the files on the µSD card.
    Files on the card
    Files on the card