SparkFun Qwiic Shield for Arduino Nano Hookup Guide

≡ Pages
Contributors: El Duderino

Hardware Overview

The Qwiic Shield for Arduino Nano is pretty straight forward shield but has a few extra bits we'll cover in this section.

Qwiic Connectors

Just like our other Qwiic adapter boards, the Qwiic Shield for Arduino Nano comes with several Qwiic connectors. There are two horizontal Qwiic connectors on the edges of the board and two vertical ones in the center.

Image highlighting Qwiic Connectors on Qwiic Shield for Arduino Nano.

Logic Shifting Circuit and IOREF Jumper

The Qwiic Shield for Arduino Nano has a configurable logic shifting circuit depending on the voltage your Arduino Nano runs at. There is a jumper on the shield to set the IOREF voltage for the logic shifting circuit. The jumper defaults to 3.3V which works fine for 33 Nanos like the Arduino 33 Nano BLE but you will need to switch the jumper to 5V for Arduino Nanos that run at 5V like the Arduino Nano Every.

Image Highlighting logic circuit for Qwiic Shield for Arduino Nano.

Never worked with solder jumpers before just need some tips or a quick refresher? Check out our How to Work with Jumpers and PCB Traces tutorial.


How to Work with Jumper Pads and PCB Traces

April 2, 2018
Handling PCB jumper pads and traces is an essential skill. Learn how to cut a PCB trace, add a solder jumper between pads to reroute connections, and repair a trace with the green wire method if a trace is damaged.

I2C Jumper

The I2C jumper pulls the Qwiic SDA and SCL lines up to 3.3V through 4.7K resistors. The reference voltage set by the IOREF Jumper has no effect on the voltage of the pull up resistors. You can disable them by severing the trace in between the pads if you have many devices on your I2C bus.

Image highlighting I2C Jumper on the Qwiic Shield for Arduino Nano.

Board Dimensions

The shield measures 1.7in. x 0.7in. (43.18mm x 17.78mm) and has four mounting holes with a 0.07in diameter that match those on the Nano footprint.

Dimensional Drawing for Qwiic Shield for Arduino Nano