SparkFun ProDriver and Mini Stepper Motor Driver Hookup Guide

≡ Pages
Contributors: QCPete, santaimpersonator

Hardware Assembly

Hardware Connections

Latch Terminals

When working with the latch terminals of the ProDriver, users should be aware of the following, about the clamping mechanism:

  1. If you look closely at the closed jaws or clamping mechanism, you will notice a small gap. Just like screw terminals, there is a minimum and maximum wire thickness for the jaws to physically clamp onto wires.
    • On some stepper motors, you may need to tin (i.e. add a little solder) the wire leads and thicken the wires just enough to be clamped.
  2. Make sure you are inserting the wire between the jaws.
    • Looking to the right end of the picture, below, on the latch partially closed, it should be noted that is possible to accidentally insert a wire above the jaws.

latching mechanism
The latching mechanism on the ProDriver. (Click to enlarge)

Headers

When prototyping, users may consider soldering headers to the ProDriver or Mini Stepper Motor Driver. Most users may consider solder headers to the Mini Stepper Motor Driver, as the pin layout is compatible with breadboards.

soldering headers
Soldering headers to the Mini Stepper Motor Driver. (Click to enlarge)

When connecting Mini Stepper Motor Drivers in parallel, users may find it more convenient to utilize our stackable headers.

stacked mini stepper motor drivers
Using stackable headers on the Mini Stepper Motor Driver. (Click to enlarge)

Hookup Wires

For a more permanent connection, user may choose to solder their connections directly to the ProDriver or Mini Stepper Motor Driver.

soldering wires
Soldering headers to the Mini Stepper Motor Driver. (Click to enlarge)

Power Connections

REMEMBER to disconnect the power before connecting/disconnecting your motor.

On the Prodriver, we recommend one of our wall adapter, power supplies to connect to the DC barrel jack. Otherwise, users can utilize the (VM and GND) PTH or latch pins to attach an external power supply.

power connection
The power connected to the ProDriver. (Click to enlarge)

On the Mini Stepper Motor Driver, users can connect an external power supply to the VM and GND PTH pins. When prototyping with a breadboard, we recommend using either the regulated power from a development board or utilizing a barrel jack adapter.

power with redboard
Powering the Mini Stepper Motor Driver with a RedBoard. (Click to Enlarge)
power with adapter
Powering the Mini Stepper Motor Driver from a DC barrel jack adapter. (Click to Enlarge)

⚡ Note: For the Mini Stepper Motor Driver, we recommend that users attach an electrolytic capacitor (>50µF) between the VM and GND pins.

Input Control Pin Connections

The input control pins need to be connected to a microcontroller. To utilize the Arduino examples below, without modifying the code, we recommend using the SparkFun RedBoard (Qwiic) as the microcontroller. Use the table and image below to hookup a SparkFun RedBoard to the ProDriver or Mini Stepper Motor Driver with some jumper wires.

microcontroller connections to the ProDriver
microcontroller connections to the Mini Steppper Motor Driver

Connecting a SparkFun RedBoard to a ProDriver or Mini Stepper Motor Driver. (Click to enlarge)

ProDriver Control Pins STBY EN MODE0 MODE1 MODE2 MODE3 ERR
Mini Stepper Motor Driver Control Pins STBY EN M0 M1 STEP/M2 DIR/M3 ERR
RedBoard Pins D8 D7 D6 D5 D4 D3 D2
Note: Don't forget to ground loop the motor driver to the RedBoard as illustrated in the image above.
Parallel Operation: When operating multiple motor drivers in parallel, all of the pin connections to the microcontroller are shared, with the exception of the MODE 1/M1 pin. Each motor driver board requires a seperate pin on the microcontroller to operate their MODE 1/M1 pin. (See the example below)

Motor Channel Output Connections

The output channels for the H-Bridges need to be connected to the stepper motor. Users need to hookup the wire pairs for each coil to individual channels. However, the polarity of the connections isn't very important as the direction of the motor rotation can be controlled in software. For the recommended stepper motor, use the table and image below to hookup the motor to the ProDriver or Mini Stepper Motor Driver.

motor connection for the ProDriver
motor connection for the Mini Steppper Motor Driver

Connecting a stepper motor to a ProDriver or Mini Stepper Motor Driver. (Click to enlarge)

Motor Driver Output Channels A+ A- B+ B-
Stepper Motor Wires Black Green Red Blue

⚡ Note: Do not connect or disconnect the motor while the motor driver is powered; as it may damage the TC78H670FTG IC.

Motor Coil Pairs

In order to determine the wire pairs for each coil on their stepper motor, users can refer to the datasheet for the stepper motor. Often, the relevant information is indicated as shown in the diagram below.

Motor Coil Diagram
Coil wire diagram from the datasheet our NEMA 16 Stepper Motor with Cable. (Click to enlarge)

For a 4-wire motor, users can alternatively use a multimeter to determine the wire pairs for the coils. This is done by comparing the resistance of one wire and against each of the three remaining wires. Whichever wire shows the lowest resistance against the first wire is the pair mate. The remaining two wires should show similar resistance between the two of them.

Examples

Single Stepper Motor

Utilizing the instructions above, an example of the standard assembly used for most of the examples in the Arduino library, is shown below.

standard setup - ProDriver
The SparkFun RedBoard connected to a ProDriver and stepper motor. (Click to enlarge)
standard setup - Mini
The SparkFun RedBoard connected to a Mini Stepper Motor Driver and stepper motor. (Click to enlarge)

ProDriver Control Pins STBY EN MODE0 MODE1 MODE2 MODE3 ERR
Mini Stepper Motor Driver Control Pins STBY EN M0 M1 STEP/M2 DIR/M3 ERR
RedBoard Pins D8 D7 D6 D5 D4 D3 D2

Multiple Stepper Motors

For users interested in utilizing multiple stepper motors, we have provided an additional Arduino example for hooking up two Mini Stepper Motor Driver(s) and/or ProDriver(s) in parallel. Use the table and image below to hookup the SparkFun RedBoard to the two motor drivers with some jumper wires.

Two ProDrivers
Two ProDrivers
Two Mini Stepper Motor Drivers
Two Mini Stepper Motor Drivers
ProDriver and Mini Stepper Motor Driver
Combination

The SparkFun RedBoard connected to two motor driver boards. (Click to enlarge)

Note: All of the pin connections to the motor drivers are shared, in parallel from the RedBoard; with the exception of the MODE 1/M1 pin. Each motor driver will utilizes a different pin on the RedBoard, for their MODE 1/M1 pin.
Motor Driver (1) STBY EN MODE0
M0
MODE1
M1
MODE2
STEP/M2
MODE3
DIR/M3
ERR
Motor Driver (2) STBY EN MODE0
M0
MODE1
M1
MODE2
STEP/M2
MODE3
DIR/M3
ERR
RedBoard D8 D7 D6 D5 D9 D4 D3 D2
Note: By connecting the motor drivers in parallel, they will need to be operated sequentially; they cannot be controlled simultaneously.