SparkFun ProDriver and Mini Stepper Motor Driver Hookup Guide

≡ Pages
Contributors: QCPete, santaimpersonator

Arduino Examples

Note: Most of the examples in the Arduino library will use a standard setup for the ProDriver or Mini Stepper Motor Driver (shown below), with the exception of the Example8_SerialMultiMotor demo code.

standard setup - ProDriver
The SparkFun RedBoard connected to a ProDriver and stepper motor. (Click to enlarge)
standard setup - Mini
The SparkFun RedBoard connected to a Mini Stepper Motor Driver and stepper motor. (Click to enlarge)

Example 1: Basic Motor Control

The first example in the Arduino library is perfect for demonstrating the basic functionality of the Mini Stepper Motor Driver/ProDriver. In the Arduino IDE, the example file can be found in the File > Examples > SparkFun ProDriver TC78H670FTG Arduino Library > Example1_Basic drop down menu. The example, utilizes the default configuration of the Arduino library and steps the motor utilizing clock-in control.

example 1 demo
Operation of the ProDriver utilizing the Example1_Basic example code.

Example 8: Serial Control - Multiple Motors

Example 8 demonstrates the operation of multiple motor drivers through a parallel connection. In the Arduino IDE, the example file can be found in the File > Examples > SparkFun ProDriver TC78H670FTG Arduino Library > Example8_SerialMultiMotor drop down menu. The example, configures the microcontroller to sequentially operate multiple ProDrivers.

example 8 demo
Operation of two ProDrivers utilizing the Example8_SerialMultiMotor example code.