SparkFun Line Follower Array Hookup Guide

≡ Pages
Contributors: MTaylor

Assembly

Assembly is super easy! Make the following connections with your microcontroller.

Signal/Description
Line Follower
Silkscreen
RedBot Mainboard
Silkscreen
RedBoard
Silkscreen
Power - 5v DC
5V
5V 5V
Ground GND GND GND
I2C Data
SDA/A4 A4 A4 or SDA
I2C Clock
A5/SCL
A5 A5 or SCL
INT(*) NC NC NC

* Note: INT pin is not required but can be connected to any input if the interrupt functionality is programmed into the SX1509 expander.


alt text

Using I2C via pins A4 and A5.

alt text

Using I2C via the dedicated SDA and SCL pins.

alt text

Connections are pin compatible with the RedBot Mainboard.

Mechanical Attachment to a Shadow Chassis

Attaching to the Shadow Chassis happens through the slot where the original three line following sensors were placed. Put 4-40 hardware through the array and hold with a finger. Hold the bolts through the slot in the shadow chassis, thumb on the 4-40 nuts, then make the electrical connections.

alt text

Hold the bolts in place with a finger

alt text

Thumb on the attaching nuts, then torque by hand or with a screwdriver

alt text

Make the electrical connections