SparkFun Edge Hookup Guide

≡ Pages
Contributors: Ell C, Liquid Soulder

Hardware Overview

Microcontroller

The Edge uses the Apollo3 Blue - the cutting-edge of high efficiency microcontrollers. This small BGA package packs quite a punch!

  • 32-bit ARM Cortex-M4F processor with Direct Memory Access
  • 48MHz CPU clock, 96MHz with TurboSPOT™
  • Extremely low-power usage: 6uA/MHz
  • 1MB Flash
  • 384KB SRAM

Apollo3 IC

Sensors

Such a formidable microcontroller would be wasted without a suite of cool sensors to use with it - that's why we've included two microphones, a 3-axis accelerometer, and a camera connector.

Microphones

The Edge board contains Micro Electro-Mechanical microphones that are hooked up to an operational amplifier with 75x gain to make the best use of the Apollo3's built-in 14-bit analog to digital converter.

The Apollo3 microcontroller can use Direct Memory Access to take audio recordings without using processor cycles - that means you can process audio while you record the next sample!

Microphones

Accelerometer

Dynamic interaction with the Edge is included right out of the gate with the onboard ST Microelectronics LIS2DH12 3-axis accelerometer. The accelerometer is on its very own dedicated I2C bus so there's no need to worry about address conflicts.

Accelerometer

Camera Connector

At the top of the board, we've included a camera connector to connect the Himax CMOS imaging camera.

Himax CMOS Imaging Camera - HM01B0 (Monochrome)

SEN-15570
Retired

Camera Connector

Connections

If you need anything else to complete your application there are plenty of ways to connect to the Edge board. Among these are the FTDI UART header, a Qwiic connector, four GPIO pins, four LEDs, and last (but not least) a CR2032 coin cell holder.

Serial UART Connection

You'll use this connector to program the Edge board, but after that you can also use it to talk to other systems that use a UART interface such as GPS or Serial LCD.

Serial UART Header Pins

If you connect via UART, you'll likely use the CH340E driver. The driver should automatically install on most operating systems. However, there is a wide range of operating systems out there. You may need to install drivers the first time you connect the chip to your computer's USB port or when there are operating system updates. For more information, check out our How to Install CH340 Drivers Tutorial.

How to Install CH340 Drivers

August 6, 2019
How to install CH340 drivers (if you need them) on Windows, Mac OS X, and Linux.

Qwiic Connector

The Apollo3 can have up to 6 independent I2C ports. We've taken advantage of that fact by exposing a fresh I2C port through a Qwiic connector, allowing you to add a chain of I2C sensors without soldering.

Qwiic Connector

Bluetooth Radio

The Apollo3 comes with hardware support for a Bluetooth Low-Energy (BLE) radio. The Edge board pairs that up with a surface mount antenna. The BLE controller and host can be configured to support up to eight simultaneous connections -- security and extended packet length are also supported.

Bluetooth Antenna

Inputs/Outputs

If all that wasn't enough there were still more pins available on the Apollo3, so we broke them out to four LEDs and four GPIO connections along the bottom edge. These are good for addition additional simple input or output capabilities to a project.

alt text

CR2032 Coin Cell Holder

To demonstrate just how efficient this microcontroller is we included a coin cell battery holder on the bottom. That means that once your application is all ready you can take it to school on a key-chain and show it off to your best friend!

Coin Cell Holder

JTAG Connector

For anyone who wants the utmost performance out of the Edge board during the development process you can use the JTAG MIPI 10 standard 1.27mm pitch 2x5 connector to hook up your debugger/programmer.

Heads up! You should connect your JTAG programmer/debugger from the bottom (coin-cell) side of the board. Look for a small white bar in silkscreen that indicates pin 1

JTAG Connector

Board Dimensions

SparkFun Edge development board is measures 1.80"x1.57" and includes has four mounting holes

SparkFun Edge Development Board

SparkFun Edge Development Board