SparkFun Blocks for Intel® Edison - Battery Block

≡ Pages
Contributors: CaseyTheRobot

Board Overview

alt text

Battery Block Functional Diagram TOP

  • USB Micro B - Provides power to the stack and the ability to recharge the battery

  • Power Switch - Removes all power from the stack other power supplies may still power the stack

  • Power LED - Illuminated when power is available on VSYS line; This may illuminate if another block supplies power

  • Power LED Jumper - If power consumption is an issue, cut the jumper to disable LED

  • Charge LED - LED is illuminated while charging; LED is off if no charge power is present or charge is complete

  • Expansion Header - The 70-pin Expansion header breaks out the functionality of the Intel Edison. This header also passes signals and power throughout the stack. These function much like an Arduino Shield.