SparkFun 5V/1A LiPo Charger/Booster Hookup Guide

≡ Pages
Contributors: MTaylor

Resources and Going Further

Now that you've successfully charging LiPos and boosting them up to 5V, the world is your oyster. Go plug something in! For more information, check out the resources below:

For inspiration, I've built a robot using two charger boosters to get 10 volts, for a bit of extra drive speed (and fun!).

Project Example

This robot is built on the with the

Or, see the Enginursday post on building a FLiR Pi Camera to see how two boosters can be used in parallel.