Setup and Using MicroPython for Beginners

≡ Pages
Contributors: Christo-boots with the-pher, Member #1919784

Suggested Development Environments

mpremote: MicroPython remote control

mpremote is a command line utility that provides tons of options for interfacing with a MicroPython board. A simple way to use it is to execute it standalone with no options. If you have installed mpremote you can simply execute mpremote in a command line to get direct access to the Python REPL on your board. A useful way to navigate the file system from this repl is to execute import os and then use the os methods. For example, os.listdir() will show everything in the current directory on your MicroPython board. os.getcwd() will print the name of the current directory and os.chdir('dir_name') will change the directory. An example of navigating around directories for a user who has installed the mpy_tmp117_web_server demo from this repository can be seen below.

C:\Users\qwiic_guy> mpremote

Connected to MicroPython at COM14
Use Ctrl-] or Ctrl-x to exit this shell
MicroPython on SparkFun IoT RedBoard RP2350 with RP2350
Type "help()" for more information.
>>>
>>>
>>> import os
>>> os.listdir()
['lib', 'static', 'tmp117_server_ap.py']
>>> os.getcwd()
'/'
>>> os.chdir('static')
>>> os.getcwd()
'/static'
>>> os.listdir()
['index.css', 'index.html', 'logo.png']

Once you have navigated to the directory containing the python script that you want to run, run it with the exec command:

>>> exec(open('your_script.py').read())

Other MicroPython development environments like the IDE's below will also provide you with a REPL where you can directly execute MicroPython commands. So skills gained from navigating the REPL directly with mpremote will carry over into other environments.

To get files from your computer onto your micropython board you can use mpremote cp or install them directly from repositories that support mip installation with mpremote mip install github:reponame for example, to install our qwiic_i2c_py driver, execute:

mpremote mip install github:sparkfun/qwiic_i2c_py

Let's walk through a quick example where we develop a program on a local code editor and then run it on a MicroPython board.

We can either develop our files first and then manually copy them over to our board (with mpremote cp) each time we want to test them, or we can "mount" a directory such that files are "shared" between the local file system and the MicroPython board.

Let's explore using mpremote mount to map a local directory onto our remote device. First create a new directory named hello_world and then open it in your code editor of choice. Now lets add our Python/MicroPython program. Add a file called print_platform.py to your hello_world directory. Paste the following code into the file:

import sys

print ("Hello from (Micro)Python! I am running on the following platform:", sys.platform)

The sys module exists both in Python and MicroPython so this code can run on both, and will let us know if we are successfully running it on an MCU. sys.platform will display your computer's OS if we interpret this program with a Python interpreter on your computer (for example on Windows it is win32 and on linux it is linux or linux2). However, if we interpret/execute it via MicroPython on your MCU, it will be the MicroPython port representing your MCU (for example for RP2350 it is rp2 and for ESP32 it is esp32).

Now, our local directory structure in our code editor should look like this:

Sublime Print Platform

If we run mpremote and use os.listdir to list the current contents on my board, we see that it is empty:

C:\Users\awesome_qwiic_user> mpremote
Connected to MicroPython at COM14
Use Ctrl-] or Ctrl-x to exit this shell

>>> import os
>>> os.listdir()
[]
>>>

Now let's mount our directory. Issue mpremote mount {path to your hello_world directory}. When we issue the command and again view the contents on our board, we see that our file has appeared!

mpremote Mount

Notice that our file print_platform.py is now accessible to us from our MicroPython board and how we have automatically been moved into a directory called /remote on the remote device that maps to the local hello_world directory.

Now let's run our file using the same exec(open('print_platform.py').read()) and see what happens.

>>> exec(open('print_platform.py').read())
Hello from (Micro)Python! I am running on the following platform: rp2

If all went well, we'll see our hello message and the name of an MCU platform (in this case RP2 for the RP2350).

You can add any number of files to the hello_world directory in a local code-editor, and modify them as you wish and the changes will be reflected "on-the-fly" in your mpremote session.

Thonny

Thonny is an IDE that provides a GUI environment with builtin support for MicroPython development. To get started, visit the Thonny Downloads page and download the correct version for your operating system. Run the installation/setup program that you just downloaded for Thonny and click through each of the setup pages by accepting the default settings and pressing Next.

Connect your board that already has MicroPython Firmware installed to your computer and then configure your interpreter by clicking the bottom right-hand corner of Thonny. If your serial drivers are up to date and your board has proper MicroPython firmware installed, clicking this interpreter box should show several MicroPython options:

Thonny Board Select

Select the version of MicroPython that makes the most sense for your board. Not sure? Select MicroPython (generic).

This will connect to your board and show a Python REPL in the "shell" tab. To run a MicroPython program, open it from the MicroPython device tab. Then press the green arrow (Run Current Script). If you ever want to stop the running program, soft reset your board, or reconnect to your board, click the red stop sign (Stop/Restart backend).

Let's run the same Python example in Thonny as we did for mpremote. Once connected to your board, via the instructions above, ensure that the View > Files option is selected from the Toolbar:

Thonny View Files

Now, in the Files tab, you should see two filel explorers, one called "This computer" for your local filesystem and one called "MicroPython device" representing the files on your board. Right click in the "MicroPython device" area and select New file....

Thonny New File Select

Lets call our new file print_platform.py. Let's copy and paste the same python code from the mpremote section above into our new file and save it. Now it should appear in our Files > MicroPython device tab:

A Thonny File

Finally, let's click on the green Run current script button and in the Shell tab we should see the expected print with a platform that matches the MCU of our MicroPython board:

Thonny Run Current Script

Thonny Shell

Remember that you can also still use the REPL directly from the Shell tab and execute MicroPython commands on your board just as if you were using mpremote.

PyCharm

PyCharm is a popular and modern Python IDE with plugin support for interfacing with MicroPython boards. PyCharm Professional is a paid version, but we suggest installing the free community version. To get started, visit the PyCharm Downloads Page and scroll down until you see the "PyCharm Community Addition" section and click the Download button. Open the setup executable that you downloaded and configure your installation. We suggest accepting the default installation folder and adding the Desktop Shortcut and Context Menu.

PyCharm Install

Once your install is complete, open PyCharm. Skip any import settings that pop up when you open it for the first time.

Navigate to Plugins and in the "Marketplace" tab search for "MicroPython Tools".

Note: This is a third-party plugin with no explicit support or maintenance from Jetbrain or SparkFun. Older versions of PyCharm contain a JetBrains-supported plugin called simply "MicroPython" but they no longer update it and it cannot run on the latest PyCharm versions.

MicroPython Tools

After installing the plugin, restart your IDE. Then, select the gear icon and choose "Settings" then navigate to Languages & Frameworks and select MicroPython Tools.

PyCharm Framework

Select Enable MicroPython support and leave the other defaults checked. SparkFun is in the process of getting stubs for SparkFun MicroPython boards added to the official repository, but in the meantime in the stubs package field, choose a generic MicroPython stubs package corresponding to your MCU. For an RP2350 or RP2040 board, we suggest the most recent version of micropython-rp2-stubs_x.xx.x. For ESP32 boards, we suggest the most recent version of micropython-esp32-stubs_x.xx.x. These stubs packages simply provide useful code-completion, highlighting, and warnings for MicroPython development.

PC MicroPython Settings

A good starting place for the use of this plugin is the MicroPython Tools README. Let's create our first project. Click the "+" sign or select file > New Project... to create a new project. Let's name our project "hello_world" and accept the default interpreter/environment:

PyCharm New Project

When our new project first opens up, it has our hello_world directory as well as several components like .venv and External Libraries that are helpful when doing regular Python Development.

PC Start Directory

But we are anything but regular. We will be using the MicroPython running on our MCU to interpret our code, not a Python interpreter installed on your computer. So you can mostly disregard these files.

Now, right click the hello_world directory and select Mark Directory as > MicroPython Sources Root. The MicroPython Tools plugin will now map this hello_world directory that exists on our computer to the root file system of our MicroPython board when we perform upload commands.

PC Sources Root

Now lets add our MicroPython program. Right click the hello_world directory and select new > Python File and add a file called print_platform.py. Paste the following code into the file:

import sys

print ("Hello from (Micro)Python! I am running on the following platform:", sys.platform)

This is the same code as is discussed in the mpremote section.

Now lets configure an upload command and a run command. At the top of PyCharm next to the execute and debug buttons, select Current File > Edit Configurations:

Edit Configurations

In the Run/Debug Configurations window that pops up, select the "+" sign and then select MicoPython Tools > Upload Project. Check the boxes for Reset on success, Switch to REPL tab on success. Then, click Apply.

PC Upload Project

While we're at it, lets create an execute command. Again, click the "+" sign and select MicroPython Tools > Execute. Input the path to our print_platform.py file we have created and check the box for Switch to REPL tab on success. Click Apply and finally OK to save our upload and execute commands.

PC Execute

The upload command will take the directory that is configured as MicroPython Sources Root (in our case the hello_world directory) and load that onto the root directory of our MicroPython connected board. The execute command will run whatever file we have selected from the local computer's file system and run it on our board (without explicitly uploading it to the device).

Now, let's connect to our device! Plug in your board that already has MicroPython Firmware installed and then in the bottom-left of PyCharm, select the MicroPython Tools extension. Select the correct COM port for your board. And then click the plug symbol to connect.

PC Connect

Now that we are connected, let's upload our program. Select our upload configuration from the drop-down at the top of PyCharm and then click the green Run arrow.

PC Run Upload

Select the File System tab in the MicroPython tools extension tab and we should now see print_platform.py file uploaded to the device!

PC File System

Finally, let's select our execute configuration and run it as well.

PC Run Execute

If all goes well, you should see a hello statement printed in the REPL tab of the MicroPython Tools extension. The platform printed should match the MCU of your board and not be your computer's operating system.

PC Running Smoothly

Some Things to Note:
  • The execute job we configured uses the version of the file currently in our local hello_world directory and runs it directly without uploading it. The upload step is helpful however if we have multiple files that we want to upload at once, for example if the file we are actually running relies on other files.
  • Drag and drop is supported by this extension, such that you can simply drag files from the project explorer on the left of PyCharm to the File System tab of the extension to copy files from your local computer to your MicroPython board.
  • Another alternative to explicitly using an upload configuration is to select a file from the PyCharm project explorer and right click it and select either Execute file in MicroPython REPL or Upload file to MicroPython device.
  • Remember that you can still use the REPL directly from the REPL tab and execute MicroPython commands on your board just as if you were using mpremote.
  • Other Tools