Setup and Using MicroPython for Beginners

≡ Pages
Contributors: Christo-boots with the-pher, Member #1919784

SBC Setup

Raspberry Pi Setup

Follow the instructions here to to download a Raspberry PI OS image. It is expected that most/all RaspberryPi OS versions will work with our Qwiic I2C drivers, but testing was done with Kernel v6.6, Debian GNU/Linux 12 (bookworm). Image an SD card with your favorite SD card imager, we recommend the Raspberry Pi Imager.

Jetson Orin Nano Setup

Follow the in-depth instructions here to set up your Jetson Orin Nano Developer kit with a JetPack 6.2 (or higher) Linux image.

Qwiic Shim or Qwiic Cable Female Jumper Setup

On either of the above platforms, a pysical hardware interface is required to connect the I2C pins of the board to a qwiic connector on a qwiic device. Connect a Qwiic Shim or a Qwiic Cable Female Jumper to your board, making sure to connect the correct pins for PWR, GND, SDA, and SCL. See the instructions here for more information. Then connect a qwiic cable to your SparkFun Qwiic Device.

Warning: IMPROPER ORIENTATION OF A QWIIC SHIM CAN SHORT POWER TO GROUND, DAMAGING YOUR BOARD!