RETIRED - Using the Logic Level Converter

This Tutorial is Retired!

This tutorial covers concepts or technologies that are no longer current. It's still here for you to read and enjoy, but may not be as useful as our newest tutorials.

View the updated tutorial: Bi-Directional Logic Level Converter Hookup Guide

≡ Pages
Contributors: jimblom

Resources and Going Further

Here are some resources related to the LLC and level-shifting in general:

Going Further

If you're looking for a place to use the LLC, these tutorials might spark some ideas:

  • Electric Imp Breakout Hookup Guide -- The Electric Imp works at 3.3V max, so if you interface it with any 5V systems you may need an LLC.
  • Getting Started with pcDuino -- The pcDuino is another 3.3V-based system. This is a powerhouse compared to the Electric Imp, though. It can run Linux or Android, and has all sorts of awesome functionality.
  • Using the Arduino Pro Mini 3.3V -- If you want to stick with Arduino, and want to use 3.3V sensors, consider using an Arduino that runs at 3.3V. That way you won't even need to bother with an LLC!