pcDuino Hookup Guide

This Tutorial is Retired!

This tutorial covers concepts or technologies that are no longer current. It's still here for you to read and enjoy, but may not be as useful as our newest tutorials.

≡ Pages
Contributors: SFUptownMaker

Introduction

This article should give you a leg up on developing a project around the pcDuino. Getting started is easy: just plug in the cables, and away you go!

ReplaceMeOpen

ReplaceMeClose

Okay, so that bit was easy. But what's next? Now that you've got the machine up and running, what do you actually do with it?

We're here to help. In the following pages, you'll find some handy mini-tutorials to add features, change settings, write code, and just generally get more out of your pcDuino. All of these things assume that you're running the standard Linux distribution that came with the pcDuino; as time goes by we'll add some content covering Android as well.

Hardware Tour

Here's a brief visual rundown of the hardware on the pcDuino.

Top side

Top side connections and hardware

  • Debugging serial port - a root-level session is initiated to this serial port at power up. It can be accessed as a 3.3V serial port, 8-N-1, no handshaking. For more information, see this page.
  • Android buttons - these duplicate the functions of the hardware buttons on many Android-based tablets and phones. In Android programming, these buttons have a special function.
  • GPIO - four 3.3V GPIO pins.
  • SPI - two dedicated SPI peripheral headers. J6 is the SPI2 peripheral; J7 is the SPI0 peripheral, which is also broken out to the appropriate pins on the Arduino-ish headers. SPI0 pins also provide access to two more UARTs and external interrupts, as well.
  • Arduino-ish headers - these pins closely follow the functionality of the pins on standard Arduino-compatible boards: I2C, SPI, UART, PWM, and ADC. The mapping is the same as it would be on a standard Arduino-compatible, as well, making it easy to convert Arduino shields to work with pcDuino.

Bottom side

Bottom side connections and hardware

  • MicroUSB power port - this port is for power only- the data pins don't connect to anything. The board uses about 500mA under normal circumstances, meaning it can be powered from most USB ports; most modern cellular phone chargers use microUSB as well, making finding a power supply easy.
  • USB-OTG port - this port can be used either as a standard USB port (with the appropriate converter) or to connect the pcDuino to another PC for debugging and upgrading the onboard software. The board can be powered through this port for debugging.

DVI Video Fix

NB: This page is out of date; please proceed to the "Changing the OS" page and follow directions there to load a new Ubuntu image onto the pcDuino which will fix the issue with display on DVI devices. This page is being left as reference, and the direction here will still work.

The first-generation pcDuino has an issue with its display setup, which causes it to fail to properly display images on some DVI monitors. In future hardware revisions, this fix will ship with the device; for now, you may need to apply it manually.

Download these files to the root directory of a USB flash drive or microSD card:

If your display is working, but the color is "off", follow these instructions:

  1. Insert the USB drive or microSD card into the pcDuino.
  2. Launch LXTerminal from the link on the pcDuino desktop.
  3. Enter the following commands at the prompt:

    cd /media/*
    sudo bash ./update_for_dvi

The patch will be applied automatically; it takes a few seconds. You should get a message stating that the pcDuino will restart in 10 seconds; after the restart, the problem should be solved.

If you cannot see the image on your display, the process is slightly more complicated. You'll need to connect to the onboard serial debugging port. For instructions on how to do this, visit this page.

Now go ahead and connect the power to the pcDuino. You should see the light next to the reset button (between the HDMI and Ethernet ports) come on, and text should start scrolling by in the console. If that doesn't happen, you may need to check the connection between your pcDuino and the serial bridge to make sure the wires are in right.

This is what you'll see when the boot process is completed.

pcDuino boot completed on a terminal

Now, follow these steps:

  1. Insert the USB drive or microSD card into the pcDuino.
  2. Enter the following commands in the terminal window:

    cd /media/*
    bash ./update_for_dvi

The patch will be applied automatically; it takes a few seconds. You should get a message stating that the pcDuino will restart in 10 seconds; after the restart, the problem should be solved.

If you have any questions or problems, please contact SparkFun technical support!

Serial Debugging

A very useful feature of the pcDuino is a 3.3V logic-level serial port, which allows access to a root-level terminal session after boot. It also delivers information about the boot process, which can be useful for troubleshooting issues occurring during boot.

Debug serial pins

Connecting to this is simple, and there are many options for doing so. Here, I'll give you instructions on using an FTDI Basic board, an FTDI cable, or an Arduino-compatible board. You'll need either some female-male jumper wires or (second best option) some male header pins and female-female jumper wires.

FTDI Basic

FTDI Basic connection

The FTDI Basic connection is easy, since the pins on the FTDI Basic board are labeled.

FTDI Cable

FTDI cable connection

The FTDI cable has no label on the connector, but the pinout is (for this use, anyway) the same as that for the FTDI Basic.

Arduino-Compatible board

Using an Arduino-compatible board as a serial bridge

This is the most difficult method for connecting to the debugging port, although probably the most readily available. The first thing you'll want to do is load a sketch (like this one) which makes the RX and TX pins inputs. That will ensure that there's no conflict between the ATmega on the Arduino-compatible and the pcDuino. Then, connect the pins from the pcDuino to the headers on the Arduino-compatible board. Unlike the other two options, in this case, you'll connect the pcDuino transmit pin to the TX pin on the Arduino-compatible and the pcDuino receive pin to the RX pin. This is because the label on the Arduino-compatible headers refers to the direction of the data relative to the ATmega, not the serial bridge device.

Terminal settings

Use your favorite terminal program (I like PuTTY); I'd strongly suggest avoiding the Arduino serial terminal function, however. You'll want to be sure local echo is off. The connection settings you'll need are:

  • 115200 baud
  • 8 data bits
  • no parity
  • 1 stop bit
  • no handshaking

Wireless Networking

The minimalist Linux installation that comes with the pcDuino supports wireless networking, but you'll have to get your hands a little dirty to get it to work. Here's a walkthrough for getting the USB wifi dongle we sell working with your pcDuino:

  1. Boot the pcDuino.
  2. Plug in the dongle.

    Finding the "Network Connections" utility

  3. Open the "Network Connections" utility, under the "Preferences" submenu in the system menu.

    Adding a wireless connection

  4. Under the "Wireless" tab, click the "Add" button.

    Configuring wireless connection

  5. You can put whatever you like in the "Connection name" field, but you'll need to have the SSID of the network you want to connect to in the SSID field. Mode should default to "Infrastructure", which is correct for most networks, and the bottom four fields can be ignored.

    Configuring wireless security

  6. In the "Wireless Security" tab, you can set the network security options for your network. We won't attempt to cover this, because it's too big a topic; the fields should be pretty similar to those on other devices, so copy the settings from something else if necessary.

  7. The last two tabs, "IPV4 Settings" and "IPV6 Settings", you can probably ignore. If you do need to use them, you likely know that you do, and you probably quit reading this page a while ago.

    Network connection creation completed

  8. Hit the "Save" button to return to the "Network Connections" utility. You'll see your new connection in the list; the "Last Used" column will say "never" next to this connection. That's okay. Go ahead and close the window and your connection should be ready to go!

Tips and Tricks

Now that you're up and running, there are a few things you may find useful to do immediately.

Change/disable screensaver timeout

The default screensaver settings will cause the monitor to blank almost immediately after boot. If that's not to your liking, here's how to change it.

  1. Open Leafpad. There's an icon on the desktop.
  2. From the "File" menu, choose the "Open..." option.
  3. The file you want is hidden, so you'll have to type the filename to open it. In the "Places" frame, click "ubuntu" to show the contents of the ubuntu user home directory. Then, click the pencil in the upper left to enable the filename entry field. Type ".xscreensaver" in the "Location:" field, and click open.

    Leafpad open file dialog

  4. The file that opens has one line:

    mode: blank

Change "blank" to "off". That will disable the screensaver entirely. Save the file, and you're done! There are more settings that can be made here; see this link for details.

Running a program at boot

Say you want to always have an LXTerminal window open when the GUI loads. How do you go about doing this?

All you need to do is add the command to the end of the autostart file located here:

/etc/xdg/lxsession/Lubuntu/autostart

For instance, to launch LXTerminal at boot, add the line "lxterm" to the end of the file.

Stopping the GUI from automatically loading on boot

If you're using a pcDuino in an embedded application, it may be helpful to prevent the GUI from loading, to conserve processor resources. To log in only as root, with access only via the debugging serial port, open this file:

/etc/lightdm/lightdm.conf

Delete all of the content after [SeatDefaults]. This will stop it from launching the window manager and logging you in.

If you only want to stop the automatic login, just remove the last line ("autologin-user=ubuntu") from the file, and you'll be presented with a login screen at reboot.

Changing the OS

The last thing you might be interested in doing is reloading or changing the operating system on the device. There are two methods for doing this: LiveSuit (sometimes found on the internet as "LiveSuite") and PhoenixCard. LiveSuit can be used to load either Lubuntu or Android; PhoenixCard can only be used to load Linux. We'll only be covering LiveSuit, as it is the easier and preferred means for doing this.

LiveSuit is available in a Windows (32-bit) version, a Windows 7 (64-bit) version, or in a Linux (64-bit-only) version. We'll skip over installation of the tool; the linked website explains how to install the Linux version, and the Windows versions don't need to be installed, merely extracted.

You'll also need the appropriate image file. This Lubuntu image is an update to the image that ships with the pcDuino, but it has some serious enhancements and bug fixes, and is well worth the upgrade. There is also an Android image available, but it hasn't received as much attention as the Lubuntu image.

Installing drivers (Windows only)

Before going any farther, you should install the drivers for the pcDuino debugging port. Make sure that you have the right version of LiveSuit--the drivers in the 32-bit version won't work on a 64-bit system!

  1. Plug a microUSB cable into your computer. While holding the button marked SW2 on your pcDuino, plug the other end of the cable into the USB-OTG port on your pcDuino.

    Labeled hardware for updating flash

  2. In Windows XP, you'll see a driver installation query pop up. In Windows 7, you'll probably have to open the device manager. The device will appear as "USB Device(VID_1f3a_PIDefe8)" under the "Universal Serial Bus controllers" section. The drivers are in the LiveSuit directory, in the "UsbDriver" directory.

    Device manager for Windows 7

  3. Once driver installation has completed, unplug the pcDuino.

Installing Android

  1. Launch the LiveSuit application.
  2. Select the Android image file you downloaded above.
  3. Plug a microUSB cable into your computer. While holding the button marked SW2 on your pcDuino, plug the other end of the cable into the USB-OTG port on your pcDuino.

    LiveSuit first format message

  4. After a few seconds, LiveSuit will popup with a window asking if you want to format the device. Since we're reflashing, choose "Yes". Note that even if mandatory doesn't format, you'll lose anything installed on the device, so back it up!

    LiveSuit second format message

  5. LiveSuit will double check that you want to format the device. Click "Yes" again.

    Update success message

  6. Click "Finish" in the next window. Don't worry about the directions in the window; they're not important. Or comprehensible.

    LiveSuit updating

  7. The progress bar will fill in, and if you've got a connection on the serial port terminal, you can watch the progress there as well. Don't be alarmed if there are some long pauses during the update, although the whole process should not take more than five minutes.

  8. LiveSuit will give you an "Update success" window, and the pcDuino will automatically reboot into Android. Note that when watching the serial debugger port output, Android doesn't give you any kind of a prompt--just a blank line, into which you can enter commands.

Installing Ubuntu

  1. Launch the LiveSuit application.
  2. Extract the Ubuntu archive you downloaded above. In it are two image files: "a10_kernel_20130203.img" and "ubuntu_20130203.img". Select the "a10_kernel_20130203.img" file.
  3. Copy the files "env_nandd.fex", "ubuntu_20130203.img", and "update.sh" from the Ubuntu directory you just extracted to either a microSD card or a flash drive. Make sure the files are in the root directory of the drive!
  4. Insert the flash drive or microSD card into the pcDuino.
  5. Plug a microUSB cable into your computer. While holding the button marked SW2 on your pcDuino, plug the other end of the cable into the USB-OTG port on your pcDuino.

    LiveSuit first format message

  6. After a few seconds, LiveSuit will popup with a window asking if you want to format the device. Since we're reflashing, choose "Yes". Note that even if mandatory doesn't format, you'll lose anything installed on the device, so back it up!

    LiveSuit second format message

  7. LiveSuit will double check that you want to format the device. Click "Yes" again.

    LiveSuit update complete

  8. Click "Finish" in the next window. Don't worry about the directions in the window; they're not important. Or comprehensible.

    LiveSuit updating

  9. The progress bar will fill in, and if you've got a connection on the serial port terminal, you can watch the progress there, as well. Don't be alarmed if there are some long pauses during the update, but it won't take more than five minutes to complete.

  10. LiveSuit will open an "Update success" message. Do not disconnect the power from the pcDuino at this time.

    Serial monitor after Ubuntu image load complete

  11. If you're connected to the serial monitor, you can watch the device update from the external memory. It takes some time--several minutes at least--and at the end, an "update complete" message will appear on the serial monitor.

  12. If you're not connected to the serial monitor, you'll know the update process is completed when the RXLED and TXLED will blink slowly, in unison. While the upgrade is underway, RX will be solid on and TX will be blinking.

  13. Once the upgrade is complete, you may restart the pcDuino.

Resources and Going Further

To learn more about the pcDuino visit our programming the pcDuino tutorial. There you'll learn how to access and use the GPIO and turn your pcDuino into a single-board computer capable of interact with the physical world.

Here are a few links that may be useful in your further exploration of the pcDuino: