RED-V Thing Plus Hookup Guide

≡ Pages
Contributors: santaimpersonator, Evan_Double_U, Englandsaurus, bboyho

Introduction

SparkFun is pleased to welcome its a whole new instruction set architecture (ISA) to its family, the RISC-V ISA (pronounced “risk-five”), and along with it, introduce the RED-V Thing Plus (pronounced “red-five”). In this tutorial, we'll be focusing on the hardware.

SparkFun RED-V Thing Plus - SiFive RISC-V FE310 SoC

DEV-15799
Retired

"The force is strong with this one." (Star Wars: A New Hope, 1977)

What sets the RISC-V ISA from the rest is that it is completely open-source; including the instruction set architecture (ISA). That means anyone can make full use the microcontroller without requiring royalties, licenses, or non-disclosure agreements (NDAs). The RED-V comes in the familiar SparkFun Thing Plus form factor and includes the SiFive Freedom E310 core, 32MB of QSPI flash, an NXP K22 ARM Cortex-M4 for USB connectivity and operating as a JTAG interface, and a Qwiic connector.

Required Materials

To follow along with this tutorial, you will need the following materials and software. You may not need everything though depending on what you have. Add it to your cart, read through the guide, and adjust the cart as necessary. Here is what you would need to get started:

USB 3.1 Cable A to C - 3 Foot

CAB-14743
$7.95

SparkFun RED-V Thing Plus - SiFive RISC-V FE310 SoC

DEV-15799
Retired
  • RED-V Thing Plus - You'll definitely need this; otherwise, you are probably on the wrong tutorial page (wink).
  • USB 3.1 Cable A to C - 3 Foot - The USB interface serves two purposes: it powers the board and allows you to upload programs to it. (You might even have a few of these in you drawer!)

You Will Also Need

To utilize all the features of the development board, you may need the following tools and accessories.

Click the buttons above to toggle the additional materials based on the tasks you
wish to perform. Feel free to modify the items in your cart to fit your needs.


Jumper Modification

If you would like to modify the jumpers on the board, you will need soldering equipment.

Solder Lead Free - 100-gram Spool

TOL-09325
$24.95

Chip Quik No-Clean Flux Pen - 10mL

TOL-14579
$8.50

Weller WLC100 Soldering Station

TOL-14228
Retired

Qwiic Example

If you would like to follow along with the examples below to interact with the physical world, you will also need the following items:

SparkFun Qwiic 12 Bit ADC - 4 Channel (ADS1015)

DEV-15334
$8.95

Qwiic Cable - 100mm

PRT-14427
Retired

Magnetic Screwdriver Set (20 Piece)

TOL-15003
Retired

Headers & Accessories

If you would like to add headers to your board, check out some of the following items:

Straight Header - Male (PTH, 0.1in., 40-Pin)

PRT-00116
$1.95

Feather Stackable Header Set

PRT-15187
$2.25

SparkFun Beginner Tool Kit

TOL-14681
Retired

Below is a sample selection of our other headers and soldering tools in our catalog. For a full selection of our available Headers or Soldering Tools, click on the associated link.

Extended GPIO Header - Female (PTH, 0.1in., 2x20-Pin, 16mm/7.30mm)

PRT-16763
$3.25

Insulated GPIO Header - Female (PTH, 0.1in., 2x20-Pin)

PRT-14017
$3.50

Extended GPIO Header - Female (PTH, 0.1in., 2x20-Pin, 13.5mm/9.80mm)

PRT-16764
$3.25

Straight Header - Male (PTH, 0.1in., 40-Pin)

PRT-00116
$1.95

PINECIL Soldering Iron Kit

KIT-24063
$119.95

PINECIL - Smart Mini Portable Soldering Iron

TOL-23913
$68.50

Soldering Iron - 60W (Adjustable Temperature)

TOL-14456
$25.95

Insulated Silicone Soldering Mat

TOL-14672
$15.95

Segger Programmers

If you would like to debug or flash your processor on your own, here are some of our SEGGER Programmers. Depending on the programmer that you use, you may need to use a combination of wire wrap and IC hooks to connect.

J-Link EDU Mini Programmer

PGM-15345
Retired

J-Link EDU Base Programmer

PGM-15346
Retired

J-Link BASE Compact Programmer

PGM-15347
Retired

Suggested Reading

Before continuing on with this tutorial, you may want to familiarize yourself with some of these topics if they’re unfamiliar to you.

How to Solder: Through-Hole Soldering

This tutorial covers everything you need to know about through-hole soldering.

Logic Levels

Learn the difference between 3.3V and 5V devices and logic levels.