Qwiic Pressure Sensor (BMP581) Hookup Guide

≡ Pages
Contributors: El Duderino

Hardware Assembly

Now that we're familiar with the Qwiic Pressure Sensor (BMP581), we can start assembling our circuit.

Qwiic/I2C Assembly

The fastest and easiest way to get started using the breakout is to connect the Qwiic connector on the breakout to a Qwiic-enabled development board like the SparkFun RedBoard Artemis with a Qwiic cable and as shown in the image below.

Completed Qwiic circuit

If you would prefer a more secure and permanent connection with the Standard size version, you can solder headers or wire to the PTH header on the board.

SPI Assembly (Standard Size Only)

Setting the breakout up to communicate with the sensor over SPI requires completely opening the ADR jumper and we recommend soldering to the PTH header to make the connections. If you are not familiar with through-hole soldering, take a read through this tutorial:

How to Solder: Through-Hole Soldering

September 19, 2013
This tutorial covers everything you need to know about through-hole soldering.

Along with tools for soldering, you'll need either some hookup wire or headers and jumper wires. Sever the trace between the "Center" and "Right" pads of the ADR jumper to tell the BMP581 to communicate using SPI. After opening this jumper, connect the BMP581 to your controller's SPI pins.

Highlighting the ADR jumper

Remember, the BMP581 operates at 3.3V logic so make sure to connect to a board running at the same logic level like the RedBoard Artemis or use a level shifter to adjust it to a safe voltage.