PiRetrocade Assembly Guide

≡ Pages
Contributors: LightningHawk

Kit Assembly

For step-by-step instructions on how to assemble the PiRetrocade, watch the video below. Then read on for more detailed instructions.

Hardware

This project really boils down to five buttons and a joy stick connected to the GPIO pins on the Raspberry Pi 3 and an SD card fully loaded with arcade software. Let's get started building this controller. Insert the SD Card into the Raspberry Pi . On top of the box, you will find blue prints for your controller layout. Use the provided hobby knife to cut holes labeled "Cut".

Note: Cut the white areas only. The lip of the buttons should rest where the dotted lines are surrounding the "cut" areas..

Buttons

Remove the switches from the arcade buttons. Unscrew the nut, and feed a button through each hole and secure the button to the box with the nut. Once they are all in place, replace the switches.

alt text

alt text

The bottom pin labeled "COM" for common or ground on the switch is ground. The single wiring harness will attach to the bottom pin on the short right side of the switch. It is labeled "NO" for normally open.

Joystick

First, figure out which switch corresponds to Up, Down, Left and Right. To do this easily, you can unscrew the bottom metal plate like this:

alt text

The switches will be exposed and you can test each direction. With the orientation shown holding the joystick to the left produces this result:

alt text

I labeled that top right switch "Left" which corresponds to GPIO Pin 7. Continue the same process for each direction and replace the bottom cover with the four screws along the outer edge.

alt text

Once you have the orientation, unscrew the red ball from the top of the joystick handle, and remove the black washer as well. Unscrew the top metal plate, and feed the joystick from under the box lid. Secure the joystick by screwing the metal plate on top of the box. You'll want to mark where those holes are and pre-cut a hole for each screw as well. Replace the black washer, and replace the red ball.

Wiring

You may have noticed some 6" strands of wire and 20 female quick disconnects. You will need a pair of crimpers or there may be a crimp tool on your wire strippers already. You will build two wiring harnesses for ground. One wiring harness will have five quick disconnects daisy chained together for the buttons, and the other will have four quick disconnects daisy chained together for each ground pin in the joystick. Then nine individual wiring harness for each button and direction on the joystick. The ground on the button switches are the lone tabs on the long side of the switch. The same goes for the joystick.

alt text

Single wiring harness with female end. You need nine of these.

alt text

Ground wiring harness for the joystick with female end. You need one and it can connect to any ground pin on the Raspberry Pi (Pins 6, 9, 14, 20, 25, 30, 34, or 39).

alt text

Ground wiring harness for the buttons with female end. You need one and it can connect to any ground pin on the Raspberry Pi (Pins 6, 9, 14, 20, 25, 30, 34, or 39).

In the video, each button and direction was labeled along with its corresponding GPIO on the box with marker. Below is a picture of the mapping. The individual wiring harnesses are attached on the tab that is labeled "NO" (Normally Open). It is also labeled pin 3 on the switch. "Enter" is used as "start" and is mapped to Pin 21. "ESC" is used to back out of games and labeled "Select" (Trying to keep traditional controller vibes) on the box and it is mapped to pin 26.

alt text

See the image below for the correct orientation.

alt text

For the power, audio and monitor cables, cut three holes in the back of the box, and feed those cables through them. I'm using a set of powered speakers for audio. Close the box, and get ready to play.

alt text