Photon OLED Shield Hookup Guide

≡ Pages
Contributors: b_e_n

OLED Shield Overview

Pin Descriptions

Since the shield does all of the work for you, there's no need to actually wire these connections - but in case you're looking at datasheets, or code for the Microview or OLED breakout, this table will give you a clue as to what the shield is doing. As always, you can check the schematic for more info.

alt text

OLED Shield Pin Photon Pin SPI Function I2C Function Notes
GND GND Ground Ground 0V
3V3 (VDD) 3V3 Power Power Should be a regulated 3.3V supply.
D1 (SDI/MOSI) A5 MOSI SDA Serial data in
D0 (SCK) A3 SCK SCL SPI and I2C clock
D2 (SDO) MISO — Can be unused in SPI mode. No function for I2C. —
D/C D6 Data / Command I2C address selection Digital pin to signal if incoming byte is a command or screen data.
RST D7 Reset Reset Active-low screen reset.
CS A2 — SPI chip select (active-low) —


Setting the Jumpers

With the board flipped over, you'll notice there are six jumpers. The majority of these jumpers are used to switch between SPI and I2C mode. As the board ships, these jumpers are set to configure the display in SPI mode.

alt text

Here's an overview of each jumper, moving from left-to-right, top-to-bottom in the picture above:

  • VD/VB -- This jumper shorts the digital power supply (VDD) to the battery power supply (VBAT). Because both of these supplies can be powered at 3.3V, an easy one-supply solution is to short them together and provide them a single supply. If you need to power the digital supply at something lower, like 1.8V, you may need to cut this jumper and provide two supplies.
  • D1/D2 -- This jumper can be used to short D1 to D2. If you want to use SPI, leave this jumper open. If you're using I2C, short the jumper. By default this jumper is open.
  • D/C -- This jumper can be used to short D/C to either 3.3V (1) or 0V (0). In I2C mode, the D/C pin sets the 7-bit address of the display. In SPI mode this jumper should be left open, as the D/C pin needs to be toggled to determine if an incoming byte is data or command.
  • BS2 and BS1 -- These pins on the OLED determine which interface you're using to control the OLED. With the two signals, there are four possible combinations:
    BS2BS1Interface
    00SPI
    01I2C
    108-bit Parallel (6800)
    118-bit Parallel (8080)
    By default, both of these jumpers are set to 0, which puts the display in SPI mode. If you want to change it to I2C mode, clear the BS1 jumper and set it to 1.

That brief overview should cover the 99% use case. Consult the schematic and the notes therein if you have any questions about jumpers or pins.