MPL3115A2 Pressure Sensor Hookup Guide

≡ Pages
Contributors: Nate

Arduino Code

The following Arduino example will get your sensor up and running quickly, and will show you current pressure in Pascals.

Note: This example assumes you are using the latest version of the Arduino IDE on your desktop. If this is your first time using Arduino, please review our tutorial on installing the Arduino IDE.

If you have not previously installed an Arduino library, please check out our installation guide.

Arduino Example Sub Menu

Load the Pressure example

Once the library is installed, open Arduino, and expand the examples menu. You should see the MPL3115A2_Pressure sub-menu. Load the "Pressure" example onto the Arduino. Open the serial terminal at 9600bps. You will see the current barometric pressure and temperature in the room!

Arduino terminal output

Pressure readings!

Load the BarometricHgInch example for an example that coverts pressure from Pascals to inches of mercury, altimeter setting adjusted. This type of pressure reading is used in the USA on Wunderground for home weather stations and aircraft.

Load the Altimeter example for an example that coverts pressure to current altitude in feet (or meters).

Explanation of Functions

The library and example code demonstrate the most popular functions supported by the MPL3115A2. Here is an explanation of all the available functions in the library:

  • myPressure.begin() gets sensor on the I2C bus.
  • myPressure.readAltitude() returns a float with meters above sea level. Ex: 1638.94
  • myPressure.readAltitudeFt() returns a float with feet above sea level. Ex: 5376.68
  • myPressure.readPressure() returns a float with barometric pressure in Pa. Ex: 83351.25
  • myPressure.readTemp() returns a float with current temperature in Celsius. Ex: 23.37
  • myPressure.readTempF() returns a float with current temperature in Fahrenheit. Ex: 73.96
  • myPressure.setModeBarometer() puts the sensor into Pascal measurement mode.
  • myPressure.setModeAltimeter() puts the sensor into altimetry mode.
  • myPressure.setModeStandy() puts the sensor into Standby mode. Required when changing CTRL1 register.
  • myPressure.setModeActive() starts taking measurements!
  • myPressure.setOversampleRate(byte) sets the # of samples from 1 to 128. See note below *
  • myPressure.enableEventFlags() sets the fundamental event flags. Required during setup.

When you call the readAltitude, readAltitudeFt, readPressure, or readTemp you will get a float with the sensor reading or an error code:

  • 1638.94 is an example of a valid reading.
  • -999 indicates that I2C timed out (512ms max). Check your connections.

Oversample settings table

Oversample settings

  • setOversampleRate(byte) receives a value from 0 to 7. Check table 59 above. Allows the user to change sample rate from 1 to 128. Increasing the sample rate significantly decreases the noise of each reading but increases the amount of time to capture each reading. A oversample of 128 will decrease noise to 1.5Pa RMS but requires 512ms per reading. The datasheet recommends oversample of 128 for basic applications.

The MPL3115A2 has a large number of features. Checkout the datasheet for more info. This library covers the fundamentals. Help us out! Please add or suggesting more features on the MPL3115A2 github repo.