LilyPad Vibe Board Hookup Guide

≡ Pages
Contributors: bboyho, Gella

Using a Button to Trigger Feedback

Note: This example assumes you are using the latest version of the Arduino IDE on your desktop. If this is your first time using Arduino, please review our tutorial on installing the Arduino IDE. If you have not previously installed an Arduino library, please check out our installation guide.

Copy the code below and paste it into your Arduino IDE. Select your board (i.e. LilyPad Arduino USB for the LilyPad USB, LilyPad USB Plus for the LilyPad USB Plus, etc.) and COM port. Finally, click the upload button to upload the demo on your Arduino.

language:c
/*
  LilyPad Vibe Board: Button Feedback
  Written by: Ho Yun "Bobby" Chan
  @ SparkFun Electronics
  Date: 1/14/2019
  https://www.sparkfun.com/products/11008

  The main code checks for a button press. If there is a button press,
  the Arduino turns on the LilyPad Vibe Board for haptic feedback.
  For a visual cue, the LED will turn on too. If not, the LED and
  motor will remain off.
*/

const int motorPin = 10;     // motor connected to PWM pin 9
const int button1Pin = A4;  // pushbutton 1 pin
const int ledPin =  13;     // LED pin

int button1State;  //check state of button press

void setup() {
  //Serial.begin(9600); //setup serial monitor, uncomment Serial.print()'s to debug
  //Serial.println("Begin LilyPad Vibe Motor Tests");

  pinMode(button1Pin, INPUT_PULLUP);//set internal pull up for button
  pinMode(ledPin, OUTPUT); //visual feedback


  //Quick Test 1: Check If LED and Motor Can Turn On

  //Serial.println("Turn LilyPad Vibe Motor And LED ON");
  //digitalWrite(ledPin, HIGH);  // turn the LED on
  analogWrite(motorPin, 255);  //turn motor
  delay(300);

  //Serial.println("Turn LilyPad Vibe Motor And LED OFF");
  //digitalWrite(ledPin, LOW);  // turn the LED off
  analogWrite(motorPin, 0);   //turn motor off
  delay(300);

  //Quick Test 2: Check Intensity of Motor (turns on at about 130
  // fade in from min to max in increments of 5 points:
  for (int fadeValue = 0 ; fadeValue <= 255; fadeValue += 5) {
    // sets the value (range from 0 to 255):
    analogWrite(motorPin, fadeValue);
    //Serial.print("LilyPad Vibe Motor Intensity = ");
    //Serial.println(fadeValue);

    // wait for 100 milliseconds to see motor
    delay(100);
  }
  // fade out from max to min in increments of 5 points:
  for (int fadeValue = 255 ; fadeValue >= 0; fadeValue -= 5) {
    // sets the value (range from 0 to 255):
    analogWrite(motorPin, fadeValue);
    //Serial.print("LilyPad Vibe Motor Intensity = ");
    //Serial.println(fadeValue);

    // wait for 100 milliseconds to see motor
    delay(100);
  }

}

void loop() {
  // Here we'll read the current pushbutton states into
  // a variable:

  // Remember that if the button is being pressed, it will be
  // connected to GND. If the button is not being pressed,
  // the pullup resistor will connect it to Vcc.

  // So the state will be LOW when it is being pressed,
  // and HIGH when it is not being pressed.

  // Now we'll use those states to control the LED.
  // Here's what we want to do:

  button1State = digitalRead(button1Pin);

  if (button1State == LOW)  // if we're pushing button 1
  {
    //Serial.println("Button has been pressed, turn LilyPad Vibe Motor And LED ON");
    digitalWrite(ledPin, HIGH);  // turn the LED on
    analogWrite(motorPin, 255);  //turn motor on
    delay(300);                  //slight delay for feedback
  }
  else
  {
    digitalWrite(ledPin, LOW);  // turn the LED
    analogWrite(motorPin, 0);   //turn motor off
    delay(300);
  }
}

After uploading, you should see the built-in LED on the LilyPad Arduino and the vibe motor turn on and off. The LilyPad Arduino will then slowly increase and decrease in intensity. The vibe motor will turn on when the Arduino's PWM output is around 130. Once we start looping in the loop() function, the LilyPad Arduino will check to see if there is a button press. If the button is pressed (i.e. or when A4 is connected to ground), the built-in LED and vibe motor will turn on. There is a slightly longer delay after this happens so there is enough time to detect when the motor is turned on as feedback. If there is no button press, both will remain off.