LilyPad Buzzer Hookup Guide

≡ Pages
Contributors: Gella

Attaching to a LilyPad Arduino

The LilyPad Buzzer has two sew tabs: Power (+) and Ground (-). Connect + to any digital I/O pin on a LilyPad Arduino and - to the - pin on the Arduino. To follow along with the code examples in this tutorial, connect the buzzer to a LilyPad Arduino as shown below. Alligator clips are useful for making temporary connections while prototyping until you are ready to sew the board into a project. When you are finished prototyping, replace the alligator clips with conductive thread traces.

alt text

If using the LilyPad Arduino Simple, LilyPad Arduino SimpleSnap, or LilyPad Main Board, connect to Pin 5.
If using the LilyPad Arduino USB, connect to Pin 2
.

alt text

If following along with a LilyPad ProtoSnap Plus the buzzer is pre-wired to Pin A3.

alt text

If following along with a LilyPad Development Simple the buzzer is pre-wired to Pin 9.

alt text

If following along with a LilyPad Development Board the buzzer is pre-wired to Pin 7.