Installing libmraa on Ubilinux for Edison

≡ Pages
Contributors: caseyd

Install Libraries

Install Dependencies

We'll be using Debian's Advanced Package Manager to install the dependencies needed for libmraa. Log in as root (or use "su" or "sudo") on your Edison and type:

apt-get update

apt-get update will update your local cache of all currently available packages in the repository.

The first dependency of this install is the PCRE development files.

apt-cache search pcre

apt-cache search does just what it sounds like -- searches apt packages. Look through the list and you should see:

libpcre3-dev - Perl 5 Compatible Regular Expression Library - development files

Looks like the right thing.

apt-get install libpcre3-dev

Now that we are familiar with installing packages from apt, let's get everything else we need for the build:

apt-get install git
apt-get install cmake
apt-get install python-dev
apt-get install swig

Build and Install mraa

libmraa is not in apt so we'll have to compile it from source. Don't worry, it's easy:

git clone https://github.com/intel-iot-devkit/mraa.git
mkdir mraa/build && cd $_
cmake .. -DBUILDSWIGNODE=OFF
make
make install
cd

Important: Make sure you run the final command, "make install" with root or "sudo."

That DBUILDSWIGNODE flag turns off node.js support, which isn't available in the version of swig in apt. If you need node.js, you can compile a newer version of swig from source (3.01+).

Update Shared Library Cache

To use the library in C or C++ programs, we need to add it to our shared library cache. With root (or using "sudo"), open up the ld.so.conf file:

nano /etc/ld.so.conf

Scroll down to the bottom of the file and add:

/usr/local/lib/i386-linux-gnu/

Your ld.so.conf file should look like this:

Appending library location in ld.so.conf

Save and exit ('Crtl-x' and 'y' with nano). Type the command (using root or "sudo"):

ldconfig

You can check to make sure that the cache was updated by typing the command:

ldconfig -p | grep mraa

You should see that the libraries have been included in the cache.

Verifying that libmraa was added to the cache

Export Library Path for Python

If you plan to use Python with mraa, you will need to export its location to the Python path. Enter the command:

export PYTHONPATH=$PYTHONPATH:$(dirname $(find /usr/local -name mraa.py))

Note that this command lets us use the mraa module for this terminal session only. If we restart the Edison, we will have to retype the command.

Optional: You can modify the .bashrc file to run the commands automatically every time the Edison starts. Open the .bashrc file with your favorite editor. For example:

nano ~/.bashrc

Scroll all the way down to the bottom of the file, and add the command from above in a new line.

export PYTHONPATH=$PYTHONPATH:$(dirname $(find /usr/local -name mraa.py))

The bottom of your .bashrc file should look like the screenshot below.

Appending export command in .bashrc

Save and exit ('Crtl-x' and 'y' with nano).

Updating Sudoers File

This part is also optional. If you installed sudo, you might notice that PYTHONPATH is not updated properly when you try to run a Python script with "sudo." For example, you might get an error like "ImportError: No module named mraa."

Open up the sudoers file:

sudo visudo

Right under the first "Defaults" line, add the following:

Defaults        env_keep += PYTHONPATH

Your sudoers file should look like the screenshot below.

Adding PYTHONPATH to the sudoers file

Save and exit ('Crtl-x' and 'y' with nano). Reboot your Edison for this to take effect.