Installing libmraa on Ubilinux for Edison

≡ Pages
Contributors: caseyd

Blink an LED

Using C

If you want to use C, create a file with your favority text editor:

nano blink.c

Copy the following code into that file:

language:c
/* Blinky test using mraa */

#include <stdio.h>
#include <unistd.h>
#include <errno.h>
#include <signal.h>
#include <stdlib.h>

#include "mraa.h"

#define LED_PIN 31

int running = 0;

void sig_handler(int signo)
{
    if ( signo == SIGINT ) {
        printf("Closing GPIO\n", LED_PIN);
        running = -1;
    }
}

int main()
{
    /* Initialize mraa */
    mraa_result_t r = MRAA_SUCCESS;
    mraa_init();

    /* Create access to GPIO pin */
    mraa_gpio_context gpio;
    gpio = mraa_gpio_init(LED_PIN);
    if ( gpio == NULL ) {
        fprintf(stderr, "Error opening GPIO\n");
        exit(1);
    }

    /* Set GPIO direction to out */
    r = mraa_gpio_dir(gpio, MRAA_GPIO_OUT);
    if ( r != MRAA_SUCCESS ) {
        mraa_result_print(r);
    }

    /* Create signal handler so we can exit gracefully */
    signal(SIGINT, sig_handler);

    /* Turn LED off and on forever until SIGINT (Ctrl+c) */
    while ( running == 0 ) {

        r = mraa_gpio_write(gpio, 0);
        if ( r != MRAA_SUCCESS ) {
            mraa_result_print(r);
        }
        sleep(1);

        r = mraa_gpio_write(gpio, 1);
        if ( r != MRAA_SUCCESS ) {
            mraa_result_print(r);
        }
        sleep(1);
    }

    /* Clean up GPIO and exit */
    r = mraa_gpio_close(gpio);
    if ( r != MRAA_SUCCESS ) {
        mraa_result_print(r);
    }

    return r;
}

Save and exit the file ('Crtl-X' and 'y' for nano). Compile the program with:

gcc blink.c -o blink -lmraa

Note the "-lmraa" that tells the compiler to include the mraa library. Run the program by typing:

./blink

Important: You need to run blink as root! If you get an error such as “Invalid GPIO pin specified” or "FATAL error, libmraa program must be run as root (EUID 0), cannot proceed" it means that you do not have permissions to modify GPIO. Either switch to root using the “su” command or run the command with “sudo” (if you have “sudo” installed).

You should see your LED start turning on and off!

Using Python

For Python, use your favorite text editor to create this simple script, called something like blink.py. For example:

nano blink.py

In that file, enter the following:

language:python
import mraa
import time

# Setup
x = mraa.Gpio(31)
x.dir(mraa.DIR_OUT)

# Loop
while True:
    x.write(1)
    time.sleep(0.5)
    x.write(0)
    time.sleep(0.5)

Save and exit the file (if you are using nano, press 'Crtl-X' and 'y').

Run it with:

python blink.py

Important: You need to run blink.py as root! If you get an error such as "ValueError: Invalid GPIO pin specified" it means that you do not have permissions to modify GPIO. Either switch to root using the "su" command or run the command with "sudo" (if you have "sudo" installed).

Blinking an LED with Debian on Edison

Probably not the first time you've made an LED blink, but maybe the first time in python on Debian!

Pin Map

You might have noticed that we used GP44 in hardware and GPIO 31 in our example code. This is because the mraa library uses a different number for the pins. If you would like to use mraa to control hardware, figure out which GPIO pins you plan to use on the table below (labeled "Edison Pin") and then use the MRAA Number in software.

Note that the "Edison Pin" numbers are the same GPIO pin numbers found on Linux in the Edison. They are also listed on the GPIO Block. The "Pinmode" allows you to change the function of each pin.

Notes:

  • Input/output voltage on the GPIO Block is 3.3V by default
  • Input/output voltage on the Arduino Breakout is 5V
  • Input/output voltage on the Mini Breadboard is 1.8V

MRAA pin map table based on Intel's IOT Dev Kit Repository

Edison Pin (Linux) Arduino Breakout Mini Breakout MRAA Number Pinmode0 Pinmode1 Pinmode2
GP12 3 J18-7 20 GPIO-12 PWM0
GP13 5 J18-1 14 GPIO-13 PWM1
GP14 A4 J19-9 36 GPIO-14
GP15 J20-7 48 GPIO-15
GP19 J18-6 19 GPIO-19 I2C-1-SCL
GP20 J17-8 7 GPIO-20 I2C-1-SDA
GP27 J17-7 6 GPIO-27 I2C-6-SCL
GP28 J17-9 8 GPIO-28 I2C-6-SDA
GP40 13 J19-10 37 GPIO-40 SSP2_CLK
GP41 10 J20-10 51 GPIO-41 SSP2_FS
GP42 12 J20-9 50 GPIO-42 SSP2_RXD
GP43 11 J19-11 38 GPIO-43 SSP2_TXD
GP44 A0 J19-4 31 GPIO-44
GP45 A1 J20-4 45 GPIO-45
GP46 A2 J19-5 32 GPIO-46
GP47 A3 J20-5 46 GPIO-47
GP48 7 J19-6 33 GPIO-48
GP49 8 J20-6 47 GPIO-49
GP77 J19-12 39 GPIO-77 SD
GP78 J20-11 52 GPIO-78 SD
GP79 J20-12 53 GPIO-79 SD
GP80 J20-13 54 GPIO-80 SD
GP81 J20-14 55 GPIO-81 SD
GP82 J19-13 40 GPIO-82 SD
GP83 J19-14 41 GPIO-83 SD
GP84 J20-8 49 GPIO-84 SD
GP109 J17-11 10 GPIO-109 SPI-5-SCK
GP110 J18-10 23 GPIO-110 SPI-5-CS0
GP111 J17-10 9 GPIO-111 SPI-5-CS1
GP114 J18-11 24 GPIO-114 SPI-5-MISO
GP115 J17-12 11 GPIO-115 SPI-5-MOSI
GP128 2 J17-14 13 GPIO-128 UART-1-CTS
GP129 4 J18-12 25 GPIO-129 UART-1-RTS
GP130 0 J18-13 26 GPIO-130 UART-1-RX
GP131 1 J19-8 35 GPIO-131 UART-1-TX
GP134 J20-3 44
GP135 J17-5 4 GPIO-135 UART
GP165 A5 J18-2 15 GPIO-165
GP182 6 J17-1 0 GPIO-182 PWM2
GP183 9 J18-8 21 GPIO-183 PWM3