Installing Board Definitions in the Arduino IDE

≡ Pages
Contributors: santaimpersonator

Installing a Third-Party Board Definition

For cores developed by third-party manufactures, Arduino has an extra installation process. Without which, a search for sparkfun in the boards manager, will yield no results:

no results
No results when searching for sparkfun.

The process requires a specific file, written in JSON format, that must be entered into the Additional Board Manager URLs field, inside of the Arduino IDE Preferences. This file provides the index of the Boards Manager with information about the third-party core, so that it can be linked and displayed accordingly.

The Arduino IDE Preferences is accessed from the File drop down menu, users can also use the Ctrl + , shortcut:

File drop down menu
File drop down menu in the Arduino IDE.

Preferences
Additional Board Manager URLs field in the Arduino IDE Preferences menu.

SparkFun maintains the Arduino cores for most or our development boards. Below, are each of the *.json files for the associated cores to be entered into the Additional Board Manager URLs field:

Note: We have since handed over maintenance of the Arduino core for our ESP line of microcontroller products, over to Espressif Systems. This was primarily due to changes in the Arduino IDE that caused conflicts in the compilation for MCUs hosted by separate parties.

There are a select number of boards in our catalog that may require a (different) .json file, to an separate Arduino core that is maintained by another manufacturer. For those boards, please refer to the datasheet and/or associated hookup guide for the link to their file or installation instructions.

Teensy: While we, now, handle the manufacturing of the Teensy development boards; PJRC still provides the software development of Teensyduino for their boards. To program these boards with the Arduino IDE, user will need to use the Teensyduino software add-on.


Arduino2.x.x:

*The Teensyduino software will be automatically installed, when users install the Teensy Arduino core with the Arduino IDE's Board Manager.

Arduino 1.8.x (Legacy Version):

As of 2025, PJRC only supports Arduino versions 1.8.5, 1.8.9, 1.8.13, 1.8.15, 1.8.16, and 1.8.19 with Teensyduino (v1.59). Users will need to manually download and install the Teensyduino software add-on for their OS.

*Users can still find the legacy Arduino cores on GitHub.

*For more information, check out the Teensyduino - Download + Install page.

To enter multiple .json files, users can click on the small, multi-window icon to the right of the field. A window will open, with a field for multiple URLs entries; make sure to separate each file with a , or new line (i.e. carriage return).

Additional Board Manager URLs window
Text field for the Additional Board Manager URLs window.

Use the COPY CODE button below to copy all of the files at once, instead of copying each file individually:

https://raw.githubusercontent.com/sparkfun/Arduino_Boards/main/IDE_Board_Manager/package_sparkfun_index.json
https://raw.githubusercontent.com/sparkfun/Arduino_Apollo3/main/package_sparkfun_apollo3_index.json
https://arduino.esp8266.com/stable/package_esp8266com_index.json
https://raw.githubusercontent.com/espressif/arduino-esp32/gh-pages/package_esp32_index.json
https://www.pjrc.com/teensy/package_teensy_index.json

After this procedure, the new cores will be available for install in the Boards Manager; common keywords are the board manufacturer, microcontroller family, or board name. Try searching for sparkfun in the boards manager:

Sparkfun's boards listed
SparkFun's cores listed in the Boards Manager.

Note: To search for the ESP32 and ESP8266 board definitions from Espressif Systems, use ESP as the keyword in the search bar.

To complete the installation process, users only need to click the INSTALL button that appears for the selected core, as in the previous section. For other, third-party cores, not maintained directly by SparkFun, please refer to the information provided by the core's author to get more specific instructions.