Illuminated Mask

Pages
Contributors: Gella
Favorited Favorite 6

Introduction

E-Textiles are a great way to add flair to your clothing and costumes, but crafting on a garment can be a challenge for your first project. Making an accessory is a great way to explore sewing circuits on a smaller scale.

For this project, we’ll be using multiple LEDs in a circuit to create an illuminated mask. Rather than stitching just one LED to the battery holder (as we did in the Glowing Pin project), we’ll use a parallel circuit to connect all of the LEDs to the battery.

Design and build time: 1 - 2 hours

alt text

This project is part of the LilyPad Sewable Electronics Kit, take a look at the other projects in the kit:

Suggested Reading

If this is your first sewable electronics project, we recommend you read our LilyPad Basics tutorial.

LilyPad Basics: E-Sewing

December 17, 2016

Learn how to use conductive thread with LilyPad components.

Materials and Tools

Let’s go over all of the things you’ll need to sew your project together.

LilyPad Sewable Electronics Kit

KIT-13927
$99.95
5

Items included in the LilyPad Sewable Electronics Kit:

alt text

You will also need:

  • Pen, marker, or chalk
  • Scissors
  • Hot glue gun (with extra glue)
  • Optional: Craft supplies for decorating (feathers, sequins, buttons, etc.)

Planning Your Project

For this project we’ll be using the Illuminated Mask templates (download below or use the templates included with your kit). If needed, download and print the provided template. Right-click the image below and choose “Save Link As” to download the template to your computer.

alt text

Right-click and choose “Save Link As” or click image to download PDF

There are two template pieces: a top layer and a bottom layer. Hold the top layer template up to your face to check for fit, and make any adjustments to the eye or nose shapes before tracing onto felt.

Using a pen or marker, trace the template shapes onto the felt. Both templates will fit on one piece of felt, but feel free to mix and match colors for your design. The electronics will attach to the top layer, while the bottom layer will be used to give the mask extra support. Set aside the bottom layer for now.

alt text

Understanding Your Circuit

To light up the mask, we will be connecting the LEDs to the battery holder with conductive thread using a parallel circuit layout. In a parallel circuit, components are connected to get the same amount of power running through them. Each LED in the mask will shine as brightly as the others by sharing a connection to the battery. Most of the e-textiles projects we make use parallel circuits.

alt text

Learn more about parallel circuits and e-textiles in our Multiple LED Circuits tutorial.

Arranging Your Circuit

Gather three LEDs (snap off of an LED panel if needed). Use the template as a guide to arrange your components on the felt, securing each piece with a dab of glue on the back to hold it in place. Double check that the (+) ends of the LEDs line up with the (+) tab of the battery holder.

alt text

Glue is hard to get a needle through and can interfere with making a strong electrical connection, so try not to get any in the sew tabs.

You can use a pen or marker to draw lines from one LilyPad piece to another to provide a path to follow when you stitch. For an erasable option, try disappearing ink pens or chalk.

alt text

Stitching It Together

If you need help sewing with conductive thread this tutorial covers the basics.

STEP 1:

Cut a long piece of conductive thread, thread the needle, and tie a knot at the end. Sew your first connection: starting from the positive sew tab of the battery holder, connect each of the three LEDs with a running stitch and three loops of conductive thread around each positive (+) sew tab. Tie and cut your thread.

Finish your line of stitching by tying a finishing knot on the last (+) sew tab and trimming any excess thread.

alt text

STEP 2:

With a new piece of thread, repeat the process for the negative side of the circuit – connecting the three LEDs’ negative sew tabs to one another and, finally, the negative sew tab on the battery holder. Tie a finishing knot, and trim any excess thread.

alt text

Installing Your Battery and Testing

Insert the coin cell battery into the battery holder with the positive, labeled as (+), side facing up. Slide the switch to ON to see the LEDs light up. Remove the battery, and then continue to the Finishing Touches section.

alt text

How to place a battery in a LilyPad Battery Holder.

Troubleshooting

With any electronics project, there are times you will have to troubleshoot if your circuit isn’t working. If your circuit isn’t lighting up, try a new battery or check that your project is switched on. Check your sewing for any loose threads or ends that may be touching other parts of your circuit and causing a short circuit. Learn more about troubleshooting your project in the LilyPad Basics: E-Sewing tutorial.

Finishing Touches

After you’ve checked your circuit, it’s time to get creative with adding some details to the mask. With the battery removed, glue the second layer of felt on the back of the mask to add some extra stability and insulate the back of the circuit.

alt text

Next, cut small holes on either side of the mask with scissors or a hole punch, and tie the elastic to hold the mask on.

alt text

Add craft supplies such as glitter, paint, or other decorative accents to enhance or hide your LEDs and stitching. If you want to cover the battery holder on the front of the mask, feathers or big buttons can add pizzazz and hide the board. Make sure you leave an opening so you can replace the battery when necessary.

Here are a few examples of creative decorations on finished masks:

Resources and Going Further

Looking for another project? Let’s move on to Project 2: Light-Up Plush in the LilyPad Sewable Electronics Kit.

Light-Up Plush

December 16, 2016

Craft a light-up plush with LilyPad LEDs controlled by pressing a button and sliding a switch in the creature's hands.

These tutorials will guide you through more advanced projects and concepts:

Insulation Techniques for e-Textiles

Learn a few different ways to protect your conductive thread and LilyPad components in your next wearables project.

Planning a Wearable Electronics Project

Tips and tricks for brainstorming and creating a wearables project.

Choosing a LilyPad Arduino for Your Project

Not sure which LilyPad Arduino is right for you? We'll discuss the features of each and help you decide.