H3LIS331DL Accelerometer Breakout Hookup Guide
Contributors:
SFUptownMaker
Resources and Going Further
Now that you've successfully got your H3LIS331DL up and running, it's time to incorporate it into your own project!
- For lower dynamic ranges (6-24g) SparkFun offers the LIS331 breakout board, which is library compatible with this one.
For more information, check out the resources below:
- Schematic
- Eagle Files (ZIP)
- H3LIS331DL Datasheet (PDF)
- Product Showcase Video
- ShawnHymel's H3LIS331_Ball_Demo.ino - Code used for the Produce Showcase Demo.
- GitHub Repo
- Arduino Library Code Repo
Need some inspiration for your next project? Check out some of these related tutorials:
The Uncertain 7-Cube
The Uncertain 7-Cube is a non-committal, less-than-helpful, but also entirely honest fortune teller. Simply ask it a yes or no question, give it a nudge, and the 7-Cube will dutifully inform you that it doesn’t have all the facts and doesn’t feel comfortable making a guess.
Accelerometer Basics
A quick introduction to accelerometers, how they work, and why they're used.
LSM9DS0 Hookup Guide
How to assemble, connect to, and use the LSM9DS0 -- an accelerometer, gyroscope, and magnetometer all-in-one.
Are You Okay? Widget
Use an Electric Imp and accelerometer to create an "Are You OK" widget. A cozy piece of technology your friend or loved one can nudge to let you know they're OK from half-a-world away.