Getting Started with the Teensy

≡ Pages
Contributors: Toni_K, MTaylor

Soldering Options

When it comes to soldering your Teensy, there are many different options available to you. IF you have not soldered before, make sure to check out the following tutorial!

How to Solder: Through-Hole Soldering

September 19, 2013
This tutorial covers everything you need to know about through-hole soldering.

Solder Directly Into Your Circuit

We generally recommend against soldering directly between any two boards you want to connect -- if something burns out or is connected incorrectly, you've set yourself up for a lot of annoying rework (and the danger of ripping a pad off of the board).

Teensy Flush on board

Soldering your Teensy directly to the board leads to a small profile, but you run the risk of needing to desolder a lot of pins!

One benefit of soldering directly to your circuit however is that it gives a very small profile for the project. If you plan on doing this, we recommend testing your circuit design with Alligator clips or Pig-tail cables before hand to verify functionality.

Solder Headers

Most users prefer using male headers on the Teensy and matching female headers on other boards into which the Teensy fits.

If you plan on using this method, you must ensure you solder the headers on straight, otherwise you're going to have a hard time inserting or removing the Teensy from other boards.

We recommend inserting headers into a breadboard and soldering the Teensy on from there.

Breadboard Teensy

Teensy 3.1 inserted in a breadboard for soldering. Half the pins are soldered and half aren't.

After you finish soldering the headers along the length of the board, your Teensy may look similar to the image below depending on your project.

Breadboard Teensy with Headers Soldered On

Teensy 3.2 inserted in a breadboard for soldering with all pins soldered along the length of the board.

Using male headers with the Teensy allows you to solder the headers on nice and straight, preventing crooked header insertion. As you can see from the images above however, if you intend to use the Teensy LC or Teensy 3.1+ on a breadboard, you cannot solder all of the headers.

Breadboard Incompatible

These pins aren't breadboard compatible!

If you've already soldered together a board that works with the Teensy LC/3.1, you can simply line your headers up in that board to hold them straight while soldering to the Teensy.

Hold Headers Straight

The male headers for the Teensy are being held straight by this Teensy Arduino Shield Adapter.

Once the headers are lined up straight, it's easy to simply 'plug' the Teensy into the headers and solder everything together.

Teensy Lined Up

You can see the Teensy lined up on the headers, waiting to be soldered.

You can also solder female headers or stackable headers onto the top of the board, allowing other boards to be plugged into the top of the Teensy.

TeensyOnBottom

Teensy with stackable female headers on top, allowing the Audio shield to be plugged in and the Teensy to fit into a breadboard.

If you do solder your headers on like this, keep in mind it may limit your access to the push button on board, requiring you to break out the reboot/reset signal from the header pin.

What about Those Additional Headers on the LC/3.1+?

Inner Headers

Inner Pins

Inner headers - what to do with those?!

There are a few options to work with these pins. You can:

a) Leave them unconnected (boring!)

b) Solder wires to the pins as you find uses for them

c/d) Solder headers on the top/bottom

If you go for options c or d, there's an easy way to solder connectors on there without driving yourself crazy attempting to solder a lonely pin by itself.

If you are using male headers, you can use pliers to push/pull one of the pins out. This will allow you to use the spacer to hold the pins straight, but will remove the non-compatible pin.

Using Pliers to modify Headers

Removing the unnecessary pin using pliers.

If you are using female headers, this method won't work, but you can still use the pliers to pull out the unnecessary pins.

Female Header modification

Simply pull the header pin out, and out of the way!

Once the header strip has been modified, simply line it up with those holes, and solder them.

SMD Headers

Both the 3.1+ and LC Teensy boards have SMD pins on the board bottom that you can solder to. If you know you will need access to these pins, we recommend that you solder the headers onto the top side of your Teensy.

If you already have another Teensy soldered, you can use this as a soldering jig to keep the headers straight, as shown below.

Headers Soldered On Top

Headers are soldered on the top of the board, enabling access to the SMD pads on the bottom.

With the headers soldered onto the Teensy this way, the user has access to all of the SMD pads on the bottom of the board. Keep in mind however, this does minimize access to the pushbutton, so balance that with your project needs.

If you need help with soldering to the SMD pads on the bottom of the board, please check out our tutorial here.

You can also check out this video for SMD soldering tips and tricks.