ESP32 Thing Power Control Shield Hookup Guide

≡ Pages
Contributors: Alex the Giant

Introduction

The ESP32 Power Control Shield offers a wide variety of options to control your next project. This shield enables the ESP32 Thing to switch up to 5A of a DC load between 5 and 28 volts.

SparkFun ESP32 Thing Power Control Shield

DEV-14155
Retired

Required Materials

The wish list below includes all of the materials that will be utilized in this tutorial:

Suggested Reading

If you aren't familiar with the following concepts, we recommend checking out these tutorials before continuing:

How to Solder: Through-Hole Soldering

This tutorial covers everything you need to know about through-hole soldering.

Motors and Selecting the Right One

Learn all about different kinds of motors and how they operate.

ESP32 Thing Hookup Guide

An introduction to the ESP32 Thing's hardware features, and a primer on using the WiFi system-on-chip in Arduino.

Beefcake Relay Control Hookup Guide

This is a guide for assembling and basic use of the Beefcake Relay Control board