Endless Runner Game

≡ Pages
Contributors: Shawn Hymel

Resources and Going Further

The code and circuit diagram for the Endless Runner Game project can be found on GitHub.

Challenges

  1. Add a difficulty modifier to the game: for every 20 points earned, the terrain moves slightly faster.
  2. Add a second button and remove the "gravity" effect (the part that causes the hero to move back to the first row after jumping). One button causes the hero to move up, and the other causes the hero to move down. This creates more of an "endless flying" game rather than "endless running." Feel free to change the hero graphic to a plane, spaceship, bird, mosquito, etc.
  3. Use an ultrasonic sensor to control the hero rather than one or more buttons. Set a threshold so that when an object (e.g., a hand) is more than 5 inches from the sensor, the hero is on the top row, and when the object is less than 5 inches from the sensor, the hero is on the bottom row.

Need some inspiration for your next project? Check out some of these related tutorials:

BadgerHack: Gaming Add-On Kit

Make a Breakout clone with the BadgerHack Gaming Add-On Kit.

PiRetrocade Assembly Guide

Build your very own retro gaming controller with a Raspberry Pi using the SparkFun PiRetrocade Kit!

Simon Says Assembly Guide

No matter what flavor of the Simon Says Through-hole Soldering Kit you've purchased, this tutorial is here to guide you through the entire build process.