Copernicus II Hookup Guide

≡ Pages
Contributors: Toni_K

Hardware Hookup

To get started communicating with the Copernicus II, you will need to connect four pins on the module: VCC, GND, TX-B, and RX-B.

For our example, we will be connecting the module to a terminal window on the computer using an 3.3V FTDI Basic Board, and will be using the GPS Antenna Embedded SMA.

Connections:

Copernicus II → 3.3V FTDI Basic

  • VCC → 3.3V
  • GND → GND
  • TX-B → RXI
  • RX-B → TXO

Take a look at the Fritzing diagram below showing the connections between the Copernicus II and the FTDI Basic based on the pin descriptions from the datasheet. In some cases, users needed to connect R2 to Vcc to operate but it should not be necessary.

Copernicus II Hookup