Continuous Rotation Servo Trigger Hookup Guide

≡ Pages
Contributors: Byron J.

Example Project

To demonstrate the usefulness of the Continuous Rotation Servo Trigger, we put a continuous rotation servo on a small camera dolly. The dolly has a whisker switch at each end, allowing it to do automated tabletop camera moves.

alt text

Lacking an old-fashioned rollerskate to dismantle for the chassis, we started with a commercial camera skate dolly.

Servo - Generic High Torque Continuous Rotation (Standard Size)

ROB-09347
$20.50

Jumper Wire - 0.1", 2-pin, 4"

PRT-10362
$1.25

SparkFun Servo Trigger - Continuous Rotation

WIG-13872
$17.50

Jumper Wire - 0.1", 2-pin, 6"

PRT-10367
$1.95

SparkFun Power Cell - LiPo Charger/Booster

PRT-11231
Retired

SparkFun RedBot Sensor - Mechanical Bumper

SEN-11999
Retired

Lithium Ion Battery - 2000mAh

PRT-08483
Retired

We also had some derelict robot parts around the workshop that we used to hold everything together. We improvised using materials we had handy and suggest that you do the same!

Build the Circuit

To start, we assembled the circuit on the workbench.

alt text

We used male and female headers to stack the Power Cell atop the Servo Trigger board.

alt text

Headers used to stack Power Cell on Servo Trigger.

The whisker switches were assembled as described in this hookup guide, with one built in right-hand orientation and the other left-handed.

The whisker switches also needed a quick electronic modification to make them compatible with the Servo Trigger. We desoldered the resistor from the PCB and replaced it with a blob of solder, so the whisker acts as a simple switch closure.

alt text

We plugged the 2 pin jumper wires into the GND and 5V pins on the switches and stuck some long pin headers through the switch contacts on the trigger PCB, so the switches could both plug in in parallel, one from above, the other from beneath.

alt text

We gave it a quick test on the bench. Each time a whicker switch closed, the motor drove the other way. The A, B, and T adjustments each had the desired effect.

Mechanical Integration

With the electronics working, we put them on the chassis.

The chassis itself consists of a platform with a couple of protruding M6 machine screws. The axles are mounted to the screws with wingnuts.

alt text

The drive mechanism for the cart is a simple slip clutch. We fashioned a double-width rubber wheel onto the servo using Actobotics 2" wheels and a pair of servo hubs. The motor was mounted to a B-type servo bracket, which was connected to the end of a 4.5" channel. The bracket was free to pivot in the end of the channel.

alt text

The bracket channel was simply placed over the axle bolt on the cart chassis. A rubber band was looped around the assembly, putting tension on the servo, so that the drive wheel gently touched one of the skate wheels.

On the other end of the cart, a 1.5" channel was placed over the other pivot. This allowed both axles on the cart to be spaced evenly, ensuring that all four skate wheels touch the tabletop. It also gave us some holes to mount the front whisker switch and a place to secure the battery and other electronics.

Testing Results

The first time out was somewhat disappointing -- the cart would drive until the first switch closed, then stall. It turns out the battery was nearly discharged! After a couple hours charging from a USB port, it behaved as expected.

We adjusted the trimmers so it drove slowly in both directions, with a medium transition time, so it wouldn't skid or jerk as it turned around.