Buck Regulator Hookup Guide

≡ Pages
Contributors: Alex the Giant, Ell C

Introduction

Who doesn't occasionally need power regulation? We certainly do, so we've designed the SparkFun Buck Regulator Breakout and the SparkFun BabyBuck Regulator Breakout to help us with just such a task.

Starring the AP63203 from Diodes Inc, both breakout boards take advantage of the 2A synchronous buck converter that has a wide input voltage range of 3.8V to 32V and fully integrated 125mΩ high-side power MOSFET/68mΩ lowside power MOSFET to provide high-efficiency step-down DC/DC conversion. All of this snuggled up in a a low-profile, TSOT26 package that's integrated into either a 1x1" or 0.4x0.5" board. For a wide variety of power management needs - grab yourself a Buck Regulator or Baby Buck Regulator and let's dive in!

SparkFun Buck Regulator Breakout - 3.3V (AP63203)

COM-18356
$7.50

SparkFun BabyBuck Regulator Breakout - 3.3V (AP63203)

COM-18357
$4.95

Required Materials

To follow along with this tutorial, you will need the following materials. You may not need everything though depending on what you have. Add it to your cart, read through the guide, and adjust the cart as necessary.

Tools

You will need a soldering iron, solder, and general soldering accessories.

Soldering Iron - 60W (Adjustable Temperature)

TOL-14456
$25.95

Solder Lead Free - 15-gram Tube

TOL-09163
$4.95

Suggested Reading

If you aren’t familiar with the following concepts, we recommend checking out these tutorials before continuing.

How to Solder: Through-Hole Soldering

This tutorial covers everything you need to know about through-hole soldering.

Logic Levels

Learn the difference between 3.3V and 5V devices and logic levels.

Electric Power

An overview of electric power, the rate of energy transfer. We'll talk definition of power, watts, equations, and power ratings. 1.21 gigawatts of tutorial fun!

Hardware Overview

AP63203

The AP63203 is a 2A, synchronous buck converter from Diodes Inc that has a wide input voltage range (3.8V to 32V) and provides high-efficiency step-down DC/DC conversion to 3.3V. Frequency Spread Spectrum (FSS) reduces EMI and a proprietary gate driver scheme resists switching node ringing without sacrificing MOSFET turn-on and turn-off times, which further erases high-frequency radiated EMI noise. Full details can be found in the datasheet.

Features:

  • VIN 3.8V to 32V
  • Up to 2A Continuous Output Current
  • 0.8V ± 1% Reference Voltage
  • 22µA Ultralow Quiescent Current
  • Switching Frequency - 1.1MHz
  • Supports Pulse Frequency Modulation (PFM)
    • Up to 80% Efficiency at 1mA Light Load
    • Up to 88% Efficiency at 5mA Light Load
  • Fixed Output Voltage - 3.3V
  • Proprietary Gate Driver Design for Best EMI Reduction
  • Frequency Spread Spectrum (FSS) to Reduce EMI
  • Precision Enable Threshold to Adjust UVLO
  • Protection Circuitry
    • Overvoltage Protection
    • Cycle-by-Cycle Peak Current Limit
    • Thermal Shutdown

AP63203 on the Buck Regulator AP63203 on the Baby Buck Regulator

Power

For the Buck Regulator, input power can be supplied in a number of ways. There are screw terminals on the right side of the board, solder pads for a barrel jack, which can be mounted on the top or bottom side of the board, and the plated through holes on the left side of the board can all be used as input. Output can be obtained via the screw terminals or the plated through holes.

Power options for the Buck Regulator

The Baby Buck sacrifices flexibility for space. Use the plated through holes for input and output power.

Plated through holes on the baby buck used for input and output

Both the Buck Regulator as well as the Baby Buck Regulator ratchet the output voltage down to 3.3V. Be mindful that thermal properties change as Vin increases.

Thermal Characteristics

One of the benefits of a buck converter over a linear regulator is their superior efficiency at stepping down the voltage. Unfortunately though, heat can still be a problem, particularly as the difference between the input and output voltage increases.

One of the trade-offs of the small size of the BabyBuck is because there is less copper to pull heat away from switching IC, the maximum output current available is reduced due to the thermal protections. Refer to the graphs below to see the how hot you can expect the AP63203 to get at various loads and supply voltages.

Baby Buck regulator thermal characteristics

Buck regulator thermal characteristics

To dissipate some of the excess heat, we've added a copper pad for a heat sink on the back of the 1" x 1" Buck Regulator Board. Use one of our small heatsinks and attach it with some thermal tape.

Heatsink Pad

Power LED and Jumper

On the 1" x 1" Buck Regulator, there is a power LED available for use.

Power LED is on the front of the Buck Regulator, below the AP63203

To disable this LED, cut the Jumper on the back of the board:

LED Jumper is to the left of the heatsink pad on the back of the Buck Regulator board

Board Outline

Buck Board Outline:

Outline and measurements of the SparkFun Buck Regulator Board

Baby Buck Board Outline:

Outline and measurements of the SparkFun Baby Buck Regulator Board

Hardware Hookup

There are three options when using the 1" x 1" Buck Regulator.

Screw terminals

To use the screw terminals, simply insert the correct wires into the screw terminal opening and gently tighten the screw for that port. Your board should look similar to the following:

Screw terminals on the right side of the Buck Regulator Board with wires inserted and screws tightened

Barrel Jack

To use a barrel jack for input, grab one of our PTH Mount Barrel Jack Connectors and solder that sucker on. It should look something like what you see here:

Barrel Jack fits to the board faceing out

PTH Pins

To use the plated through holes on either the Buck Regulator or the Baby Buck Regulator, you'll need to solder either straight headers or angle headers to the board.

Headers soldered to the PTH pins on both the Buck Regulator and the Baby Buck Regulator

Troubleshooting

Resources and Going Further

For more information, check out the resources below:

Buck Regulator:

Baby Buck Regulator:

Need some inspiration for your next project? Check out some of these related tutorials:

Measuring Internal Resistance of Batteries

Classroom STEM activity that has students build a battery from a lemon, measure the open and closed circuit voltages, and determine the battery's internal resistance.

Qwiic Quad Relay Hookup Guide

SparkFun’s Qwiic Quad Relay is a product designed for switching not one but four high powered devices from your Arduino or other low powered microcontroller using I2C.

TPL5110 Nano Power Timer Hookup Guide

The TPL5110 Nano Power Timer is ideal for applications that require low power, and especially those projects that are running off of a LiPo battery. The Nano Power Timer will turn on your project after the set amount of time, continuously.

How to Run a 5V Device On a 3.3V System With Qwiic

Power up your 5V I2C devices on the Qwiic system! This tutorial shows you how to use the SparkFun Qwiic 5V Boost to integrate power-hungry sensors like the SEN55 seamlessly.