Bubble Display Hookup Guide

This Tutorial is Retired!

This tutorial covers concepts or technologies that are no longer current. It's still here for you to read and enjoy, but may not be as useful as our newest tutorials.

≡ Pages
Contributors: Joel_E_B

Firmware

Before you can start writing code to control the bubble displays, you'll need to install the SevSeg Arduino Library first. You can download it from the GitHub repo. If you need more details on installing a library, visit our Installing an Arduino Library tutorial, and, if you are unfamiliar with GitHub, there's a tutorial for that too.

Once the library is installed, we can use the included example sketches to get started using the bubble display.

Example 1: Counter

Go to File -> Examples -> SevSeg -> Example -> Bubble_Display_Counter.

Here is the code for those who would like to see it without downloading it.

language:c
/*
 March 6, 2014
 Spark Fun Electronics
 Nathan Seidle
 Updates by Joel Bartlett

 This code is originally based Dean Reading's Library deanreading@hotmail.com
 http://arduino.cc/playground/Main/SevenSegmentLibrary
 He didn't have a license on it so I hope he doesn't mind me making it public domain: 
 This code is public domain but you buy me a beer if you use this and we meet someday (Beerware license).

 This sketch provides a simple counter example for the HP Bubble display from SparkFun.
 https://www.sparkfun.com/products/12710

 Pinout for HP Bubble Display:
 1:  Cathode 1
 2:  Anode E
 3:  Anode C
 4:  Cathode 3
 5:  Anode dp
 6:  Cathode 4
 7:  Anode G
 8:  Anode D
 9:  Anode F
 10: Cathode 2
 11: Anode B
 12: Anode A
 */

#include "SevSeg.h"

//Create an instance of the object.
SevSeg myDisplay;

//Create global variables
unsigned long timer;
int deciSecond = 0;

void setup()
{

  int displayType = COMMON_CATHODE; //Your display is either common cathode or common anode


  //This pinout is for a bubble dispaly
   //Declare what pins are connected to the GND pins (cathodes)
   int digit1 = 8; //Pin 1
   int digit2 = 5; //Pin 10
   int digit3 = 11; //Pin 4
   int digit4 = 13; //Pin 6

   //Declare what pins are connected to the segments (anodes)
   int segA = 7; //Pin 12
   int segB = 6; //Pin 11
   int segC = 10; //Pin 3
   int segD = 3; //Pin 8
   int segE = 9; //Pin 2
   int segF = 4; //Pin 9
   int segG = 2; //Pin 7
   int segDP= 12; //Pin 5

  int numberOfDigits = 4; //Do you have a 1, 2 or 4 digit display?

  myDisplay.Begin(displayType, numberOfDigits, digit1, digit2, digit3, digit4, segA, segB, segC, segD, segE, segF, segG, segDP);

  myDisplay.SetBrightness(100); //Set the display to 100% brightness level

  timer = millis();
}

void loop()
{
  //Example ways of displaying a decimal number
  char tempString[10]; //Used for sprintf
  sprintf(tempString, "%4d", deciSecond); //Convert deciSecond into a string that is right adjusted
  //sprintf(tempString, "%d", deciSecond); //Convert deciSecond into a string that is left adjusted
  //sprintf(tempString, "%04d", deciSecond); //Convert deciSecond into a string with leading zeros
  //sprintf(tempString, "%4d", deciSecond * -1); //Shows a negative sign infront of right adjusted number
  //sprintf(tempString, "%4X", deciSecond); //Count in HEX, right adjusted

  //Produce an output on the display
  myDisplay.DisplayString(tempString, 0); //(numberToDisplay, decimal point location)

  //Other examples
  //myDisplay.DisplayString(tempString, 0); //Display string, no decimal point
  //myDisplay.DisplayString("-23b", 3); //Display string, decimal point in third position

  //Check if 10ms has elapsed
  if (millis() - timer >= 100)
  {
    timer = millis();
    deciSecond++;
  }

  delay(5);
}

With this sketch uploaded, the display with count up, with each order of magnitude spilling onto the next digit to the left.

Example 2: Text

The next example shows how to display text. Since these display are 7-segment and not alphanumeric, they are limited in which characters they can and can't display. The sketch has a table listing all there characters and whether or not they can be displayed.

To open this sketch, go to File -> Examples -> SevSeg -> Example -> Bubble_Display_Text.

language:c
/*
 March 6, 2014
 Spark Fun Electronics
 Nathan Seidle
 Updates by Joel Bartlett

 This code is originally based Dean Reading's Library deanreading@hotmail.com
 http://arduino.cc/playground/Main/SevenSegmentLibrary
 He didn't have a license on it so I hope he doesn't mind me making it public domain: 
 This code is public domain but you buy me a beer if you use this and we meet someday (Beerware license).

The example shows you how to display characters to the bubble display. Since this is a 7-segment display
and not an alpha-numeric display, there are numerous characters that cannot be displayed. The table below 
should give you an idea which ones can. 


 Pinout for HP Bubble Display:
 1:  Cathode 1
 2:  Anode E
 3:  Anode C
 4:  Cathode 3
 5:  Anode dp
 6:  Cathode 4
 7:  Anode G
 8:  Anode D
 9:  Anode F
 10: Cathode 2
 11: Anode B
 12: Anode A

 Here is the character map found in the SevSeg.h file for reference 
 as to which characters can be displayed and which can't. 

 //  ABCDEFG  Segments
  0b1111110, // 0
  0b0110000, // 1
  0b1101101, // 2
  0b1111001, // 3
  0b0110011, // 4
  0b1011011, // 5
  0b1011111, // 6
  0b1110000, // 7
  0b1111111, // 8
  0b1111011, // 9
  0b1110111, // 10  "A"
  0b0011111, // 11  "B"
  0b1001110, // 12  "C"
  0b0111101, // 13  "D"
  0b1001111, // 14  "E"
  0b1000111, // 15  "F"
  0b0000000, // 16  NO DISPLAY
  0b0000000, // 17  NO DISPLAY
  0b0000000, // 18  NO DISPLAY
  0b0000000, // 19  NO DISPLAY
  0b0000000, // 20  NO DISPLAY
  0b0000000, // 21  NO DISPLAY
  0b0000000, // 22  NO DISPLAY
  0b0000000, // 23  NO DISPLAY
  0b0000000, // 24  NO DISPLAY
  0b0000000, // 25  NO DISPLAY
  0b0000000, // 26  NO DISPLAY
  0b0000000, // 27  NO DISPLAY
  0b0000000, // 28  NO DISPLAY
  0b0000000, // 29  NO DISPLAY
  0b0000000, // 30  NO DISPLAY
  0b0000000, // 31  NO DISPLAY
  0b0000000, // 32 ' '
  0b0000000, // 33 '!'  NO DISPLAY
  0b0100010, // 34 '"'
  0b0000000, // 35 '#'  NO DISPLAY
  0b0000000, // 36 '$'  NO DISPLAY
  0b0000000, // 37 '%'  NO DISPLAY
  0b0000000, // 38 '&'  NO DISPLAY
  0b0100000, // 39 '''
  0b1001110, // 40 '('
  0b1111000, // 41 ')'
  0b0000000, // 42 '*'  NO DISPLAY
  0b0000000, // 43 '+'  NO DISPLAY
  0b0000100, // 44 ','
  0b0000001, // 45 '-'
  0b0000000, // 46 '.'  NO DISPLAY
  0b0000000, // 47 '/'  NO DISPLAY
  0b1111110, // 48 '0'
  0b0110000, // 49 '1'
  0b1101101, // 50 '2'
  0b1111001, // 51 '3'
  0b0110011, // 52 '4'
  0b1011011, // 53 '5'
  0b1011111, // 54 '6'
  0b1110000, // 55 '7'
  0b1111111, // 56 '8'
  0b1111011, // 57 '9'
  0b0000000, // 58 ':'  NO DISPLAY
  0b0000000, // 59 ';'  NO DISPLAY
  0b0000000, // 60 '<'  NO DISPLAY
  0b0000000, // 61 '='  NO DISPLAY
  0b0000000, // 62 '>'  NO DISPLAY
  0b0000000, // 63 '?'  NO DISPLAY
  0b0000000, // 64 '@'  NO DISPLAY
  0b1110111, // 65 'A'
  0b0011111, // 66 'B'
  0b1001110, // 67 'C'
  0b0111101, // 68 'D'
  0b1001111, // 69 'E'
  0b1000111, // 70 'F'
  0b1011110, // 71 'G'
  0b0110111, // 72 'H'
  0b0110000, // 73 'I'
  0b0111000, // 74 'J'
  0b0000000, // 75 'K'  NO DISPLAY
  0b0001110, // 76 'L'
  0b0000000, // 77 'M'  NO DISPLAY
  0b0010101, // 78 'N'
  0b1111110, // 79 'O'
  0b1101111, // 80 'P'
  0b1110011, // 81 'Q'
  0b0000101, // 82 'R'
  0b1011011, // 83 'S'
  0b0001111, // 84 'T'
  0b0111110, // 85 'U'
  0b0000000, // 86 'V'  NO DISPLAY
  0b0000000, // 87 'W'  NO DISPLAY
  0b0000000, // 88 'X'  NO DISPLAY
  0b0111011, // 89 'Y'
  0b0000000, // 90 'Z'  NO DISPLAY
  0b1001110, // 91 '['
  0b0000000, // 92 '\'  NO DISPLAY
  0b1111000, // 93 ']'
  0b0000000, // 94 '^'  NO DISPLAY
  0b0001000, // 95 '_'
  0b0000010, // 96 '`'
  0b1110111, // 97 'a' SAME AS CAP
  0b0011111, // 98 'b' SAME AS CAP
  0b0001101, // 99 'c'
  0b0111101, // 100 'd' SAME AS CAP
  0b1101111, // 101 'e'
  0b1000111, // 102 'f' SAME AS CAP
  0b1011110, // 103 'g' SAME AS CAP
  0b0010111, // 104 'h'
  0b0010000, // 105 'i'
  0b0111000, // 106 'j' SAME AS CAP
  0b0000000, // 107 'k'  NO DISPLAY
  0b0110000, // 108 'l'
  0b0000000, // 109 'm'  NO DISPLAY
  0b0010101, // 110 'n' SAME AS CAP
  0b0011101, // 111 'o'
  0b1100111, // 112 'p' SAME AS CAP
  0b1110011, // 113 'q' SAME AS CAP
  0b0000101, // 114 'r' SAME AS CAP
  0b1011011, // 115 's' SAME AS CAP
  0b0001111, // 116 't' SAME AS CAP
  0b0011100, // 117 'u'
  0b0000000, // 118 'b'  NO DISPLAY
  0b0000000, // 119 'w'  NO DISPLAY
  0b0000000, // 120 'x'  NO DISPLAY
  0b0000000, // 121 'y'  NO DISPLAY
  0b0000000, // 122 'z'  NO DISPLAY
  0b0000000, // 123 '0b'  NO DISPLAY
  0b0000000, // 124 '|'  NO DISPLAY
  0b0000000, // 125 ','  NO DISPLAY
  0b0000000, // 126 '~'  NO DISPLAY
  0b0000000, // 127 'DEL'  NO DISPLAY
 */

#include "SevSeg.h"

//Create an instance of the object.
SevSeg myDisplay;

//Create global variables
unsigned long timer;
int deciSecond = 0;

void setup()
{

  int displayType = COMMON_CATHODE; //Your display is either common cathode or common anode


  //This pinout is for a bubble dispaly
   //Declare what pins are connected to the GND pins (cathodes)
   int digit1 = 8; //Pin 1
   int digit2 = 5; //Pin 10
   int digit3 = 11; //Pin 4
   int digit4 = 13; //Pin 6

   //Declare what pins are connected to the segments (anodes)
   int segA = 7; //Pin 12
   int segB = 6; //Pin 11
   int segC = 10; //Pin 3
   int segD = 3; //Pin 8
   int segE = 9; //Pin 2
   int segF = 4; //Pin 9
   int segG = 2; //Pin 7
   int segDP= 12; //Pin 5

  int numberOfDigits = 4; //Do you have a 1, 2 or 4 digit display?

  myDisplay.Begin(displayType, numberOfDigits, digit1, digit2, digit3, digit4, segA, segB, segC, segD, segE, segF, segG, segDP);

  myDisplay.SetBrightness(100); //Set the display to 100% brightness level

  timer = millis();
}

void loop()
{
  char tempString[5] = {'C','O','D','E'}; //Used for sprintf

  for(int i =0;i<100;i++)
  {

  myDisplay.DisplayString(tempString, 0); //(numberToDisplay, decimal point location)

  delay(10);
  }

   for(int i =0;i<100;i++)
  {
      tempString[0] = 58; 
      tempString[1] = 'I';
      tempString[2] = 'S';
      tempString[3] = 58;

      myDisplay.DisplayString(tempString, 0);

      delay(10);
  }
   for(int i =0;i<100;i++)
  {
      tempString[0] = 'C'; 
      tempString[1] = 'O';
      tempString[2] = 'O';
      tempString[3] = 'L';

      myDisplay.DisplayString(tempString, 0);

      delay(10);
  }

}

Example 3: Sensor Data

This last example is more of a real-world application. By adding a temperature and humidity sensor to the RedBoard, we can make a tiny, digital thermometer and hygrometer.

First, you need to add a SHT15 to your circuit. You may use whatever sensors you like, but you will need to alter the code accordingly.

alt text

Click for larger view.

Now, go to File -> Examples -> SevSeg -> Example -> Bubble_Display_SHT15 to open up the sketch.

language:c
/*
 March 6, 2014
 Spark Fun Electronics
 Nathan Seidle
 Updates by Joel Bartlett

 This code is originally based Dean Reading's Library deanreading@hotmail.com
 http://arduino.cc/playground/Main/SevenSegmentLibrary
 He didn't have a license on it so I hope he doesn't mind me making it public domain: 
 This code is public domain but you buy me a beer if you use this and we meet someday (Beerware license).

This example gives you a real world scenario in which we take sensor data (in this case temperature and humidity
data from a SHT15) and print it to the bubble display using characters and numbers. 


 Pinout for HP Bubble Display:
 1:  Cathode 1
 2:  Anode E
 3:  Anode C
 4:  Cathode 3
 5:  Anode dp
 6:  Cathode 4
 7:  Anode G
 8:  Anode D
 9:  Anode F
 10: Cathode 2
 11: Anode B
 12: Anode A

 Pinout for SHT15:
 Vcc: 3.3V
 Data: A4 or SDA on newer Arduino boards
 SCK: A5 or SCK on newer Arduino boards 
 GND: GND

 Here is the character map found in the SevSeg.h file for reference 
 as to which characters can be displayed and which can't. 

 //  ABCDEFG  Segments
  0b1111110, // 0
  0b0110000, // 1
  0b1101101, // 2
  0b1111001, // 3
  0b0110011, // 4
  0b1011011, // 5
  0b1011111, // 6
  0b1110000, // 7
  0b1111111, // 8
  0b1111011, // 9
  0b1110111, // 10  "A"
  0b0011111, // 11  "B"
  0b1001110, // 12  "C"
  0b0111101, // 13  "D"
  0b1001111, // 14  "E"
  0b1000111, // 15  "F"
  0b0000000, // 16  NO DISPLAY
  0b0000000, // 17  NO DISPLAY
  0b0000000, // 18  NO DISPLAY
  0b0000000, // 19  NO DISPLAY
  0b0000000, // 20  NO DISPLAY
  0b0000000, // 21  NO DISPLAY
  0b0000000, // 22  NO DISPLAY
  0b0000000, // 23  NO DISPLAY
  0b0000000, // 24  NO DISPLAY
  0b0000000, // 25  NO DISPLAY
  0b0000000, // 26  NO DISPLAY
  0b0000000, // 27  NO DISPLAY
  0b0000000, // 28  NO DISPLAY
  0b0000000, // 29  NO DISPLAY
  0b0000000, // 30  NO DISPLAY
  0b0000000, // 31  NO DISPLAY
  0b0000000, // 32 ' '
  0b0000000, // 33 '!'  NO DISPLAY
  0b0100010, // 34 '"'
  0b0000000, // 35 '#'  NO DISPLAY
  0b0000000, // 36 '$'  NO DISPLAY
  0b0000000, // 37 '%'  NO DISPLAY
  0b0000000, // 38 '&'  NO DISPLAY
  0b0100000, // 39 '''
  0b1001110, // 40 '('
  0b1111000, // 41 ')'
  0b0000000, // 42 '*'  NO DISPLAY
  0b0000000, // 43 '+'  NO DISPLAY
  0b0000100, // 44 ','
  0b0000001, // 45 '-'
  0b0000000, // 46 '.'  NO DISPLAY
  0b0000000, // 47 '/'  NO DISPLAY
  0b1111110, // 48 '0'
  0b0110000, // 49 '1'
  0b1101101, // 50 '2'
  0b1111001, // 51 '3'
  0b0110011, // 52 '4'
  0b1011011, // 53 '5'
  0b1011111, // 54 '6'
  0b1110000, // 55 '7'
  0b1111111, // 56 '8'
  0b1111011, // 57 '9'
  0b0000000, // 58 ':'  NO DISPLAY
  0b0000000, // 59 ';'  NO DISPLAY
  0b0000000, // 60 '<'  NO DISPLAY
  0b0000000, // 61 '='  NO DISPLAY
  0b0000000, // 62 '>'  NO DISPLAY
  0b0000000, // 63 '?'  NO DISPLAY
  0b0000000, // 64 '@'  NO DISPLAY
  0b1110111, // 65 'A'
  0b0011111, // 66 'B'
  0b1001110, // 67 'C'
  0b0111101, // 68 'D'
  0b1001111, // 69 'E'
  0b1000111, // 70 'F'
  0b1011110, // 71 'G'
  0b0110111, // 72 'H'
  0b0110000, // 73 'I'
  0b0111000, // 74 'J'
  0b0000000, // 75 'K'  NO DISPLAY
  0b0001110, // 76 'L'
  0b0000000, // 77 'M'  NO DISPLAY
  0b0010101, // 78 'N'
  0b1111110, // 79 'O'
  0b1101111, // 80 'P'
  0b1110011, // 81 'Q'
  0b0000101, // 82 'R'
  0b1011011, // 83 'S'
  0b0001111, // 84 'T'
  0b0111110, // 85 'U'
  0b0000000, // 86 'V'  NO DISPLAY
  0b0000000, // 87 'W'  NO DISPLAY
  0b0000000, // 88 'X'  NO DISPLAY
  0b0111011, // 89 'Y'
  0b0000000, // 90 'Z'  NO DISPLAY
  0b1001110, // 91 '['
  0b0000000, // 92 '\'  NO DISPLAY
  0b1111000, // 93 ']'
  0b0000000, // 94 '^'  NO DISPLAY
  0b0001000, // 95 '_'
  0b0000010, // 96 '`'
  0b1110111, // 97 'a' SAME AS CAP
  0b0011111, // 98 'b' SAME AS CAP
  0b0001101, // 99 'c'
  0b0111101, // 100 'd' SAME AS CAP
  0b1101111, // 101 'e'
  0b1000111, // 102 'f' SAME AS CAP
  0b1011110, // 103 'g' SAME AS CAP
  0b0010111, // 104 'h'
  0b0010000, // 105 'i'
  0b0111000, // 106 'j' SAME AS CAP
  0b0000000, // 107 'k'  NO DISPLAY
  0b0110000, // 108 'l'
  0b0000000, // 109 'm'  NO DISPLAY
  0b0010101, // 110 'n' SAME AS CAP
  0b0011101, // 111 'o'
  0b1100111, // 112 'p' SAME AS CAP
  0b1110011, // 113 'q' SAME AS CAP
  0b0000101, // 114 'r' SAME AS CAP
  0b1011011, // 115 's' SAME AS CAP
  0b0001111, // 116 't' SAME AS CAP
  0b0011100, // 117 'u'
  0b0000000, // 118 'b'  NO DISPLAY
  0b0000000, // 119 'w'  NO DISPLAY
  0b0000000, // 120 'x'  NO DISPLAY
  0b0000000, // 121 'y'  NO DISPLAY
  0b0000000, // 122 'z'  NO DISPLAY
  0b0000000, // 123 '0b'  NO DISPLAY
  0b0000000, // 124 '|'  NO DISPLAY
  0b0000000, // 125 ','  NO DISPLAY
  0b0000000, // 126 '~'  NO DISPLAY
  0b0000000, // 127 'DEL'  NO DISPLAY

  SHT15 code based on the code found at Wiring.org
  http://wiring.org.co/learning/basics/humiditytemperaturesht15.html

 */


#include "SevSeg.h"

//Create an instance of the object.
SevSeg myDisplay;

int temperatureCommand  = B00000011;  // command used to read temperature 
int humidityCommand = B00000101;  // command used to read humidity 

int clockPin = A5;  // pin used for clock 
int dataPin  = A4;  // pin used for data 
int ack;  // track acknowledgment for errors 
int val;  
float tempF;          
float humidity; 
float tempC;

char tempString[5];
//-------------------------------------------------------------------------------------------
void setup()
{
 int displayType = COMMON_CATHODE; //Your display is either common cathode or common anode

//This pinout is for a bubble dispaly
   //Declare what pins are connected to the GND pins (cathodes)
   int digit1 = 8; //Pin 1
   int digit2 = 5; //Pin 10
   int digit3 = 11; //Pin 4
   int digit4 = 13; //Pin 6

   //Declare what pins are connected to the segments (anodes)
   int segA = 7; //Pin 12
   int segB = 6; //Pin 11
   int segC = 10; //Pin 3
   int segD = 3; //Pin 8
   int segE = 9; //Pin 2
   int segF = 4; //Pin 9
   int segG = 2; //Pin 7
   int segDP= 12; //Pin 5

  int numberOfDigits = 4; //Do you have a 1, 2 or 4 digit display?

  myDisplay.Begin(displayType, numberOfDigits, digit1, digit2, digit3, digit4, segA, segB, segC, segD, segE, segF, segG, segDP);

  myDisplay.SetBrightness(100); //Set the display to 100% brightness level
}
//-------------------------------------------------------------------------------------------
void loop()
{

  sht15();
  clear();
  for(int i =0;i<500;i++)
  {
      tempString[0] = 'T'; 
      tempString[1] = 'F';

      myDisplay.DisplayString(tempString, 0);

    sprintf(tempString, "%4d",  (long)tempF, DEC);
    myDisplay.DisplayString(tempString, 0);
  }
  clear();
   for(int i =0;i<500;i++)
  {
      tempString[0] = 'R'; 
      tempString[1] = 'H';

    myDisplay.DisplayString(tempString, 0);

    sprintf(tempString, "%4d",  (long)humidity, DEC);
    myDisplay.DisplayString(tempString, 0);
  }
}
//-------------------------------------------------------------------------------------------
void clear()
{
      //write a non-displayable character to each position to clear the display
      tempString[0] = 'm'; 
      tempString[1] = 'm';
      tempString[2] = 'm';
      tempString[3] = 'm';

      myDisplay.DisplayString(tempString, 0);
}
//-------------------------------------------------------------------------------------------
int sht15()
{
  // read the temperature and convert it to centigrades 
  sendCommandSHT(temperatureCommand, dataPin, clockPin); 
  waitForResultSHT(dataPin); 
  val = getData16SHT(dataPin, clockPin); 
  skipCrcSHT(dataPin, clockPin); 
  tempC = (float)val * 0.01 - 40; 
  tempF = (float)tempC * 1.8 + 32;

  //Serial.print("Temperature: "); 
  //Serial.print((long)tempF, DEC);
  //Serial.print("_"); 
  //Serial.print((char)176); 
  //Serial.print("F "); 

  // read the humidity 
  sendCommandSHT(humidityCommand, dataPin, clockPin); 
  waitForResultSHT(dataPin); 
  val = getData16SHT(dataPin, clockPin); 
  skipCrcSHT(dataPin, clockPin); 
  humidity = -4.0 + 0.0405 * val + -0.0000028 * val * val; 

  //Serial.print(" Relative Humidity: "); 
  //Serial.print((long)humidity, DEC); 
   //Serial.println("%");
  //delay(1000); // wait for 3 sec for next reading 
  return tempF, tempC, humidity;
}


// commands for reading/sending data to a SHTx sensor 

int shiftIn(int dataPin, int clockPin, int numBits) { 
  int ret = 0; 

  for (int i=0; i<numBits; ++i) { 
    digitalWrite(clockPin, HIGH); 
    //delay(10); not needed :) 
    ret = ret*2 + digitalRead(dataPin); 
    digitalWrite(clockPin, LOW); 
  } 
  return(ret); 
} 

// send a command to the SHTx sensor 
void sendCommandSHT(int command, int dataPin, int clockPin) { 
  int ack; 

  // transmission start 
  pinMode(dataPin, OUTPUT); 
  pinMode(clockPin, OUTPUT); 
  digitalWrite(dataPin, HIGH); 
  digitalWrite(clockPin, HIGH); 
  digitalWrite(dataPin, LOW); 
  digitalWrite(clockPin, LOW); 
  digitalWrite(clockPin, HIGH); 
  digitalWrite(dataPin, HIGH); 
  digitalWrite(clockPin, LOW); 

  // shift out the command (the 3 MSB are address and must be 000, the last 5 bits are the command) 
  shiftOut(dataPin, clockPin, MSBFIRST, command); 

  // verify we get the right ACK 
  digitalWrite(clockPin, HIGH); 
  pinMode(dataPin, INPUT); 
  ack = digitalRead(dataPin); 
  if (ack != LOW) 
    Serial.println("ACK error 0"); 
  digitalWrite(clockPin, LOW); 
  ack = digitalRead(dataPin); 
  if (ack != HIGH) 
    Serial.println("ACK error 1"); 
} 

// wait for the SHTx answer 
void waitForResultSHT(int dataPin) { 
  int ack; 

  pinMode(dataPin, INPUT); 
  for(int i=0; i<100; ++i) { 
    delay(10); 
    ack = digitalRead(dataPin); 
    if (ack == LOW) 
      break; 
  } 
  if (ack == HIGH) 
    Serial.println("ACK error 2"); 
} 

// get data from the SHTx sensor 
int getData16SHT(int dataPin, int clockPin) { 
  int val; 

  // get the MSB (most significant bits) 
  pinMode(dataPin, INPUT); 
  pinMode(clockPin, OUTPUT); 
  val = shiftIn(dataPin, clockPin, 8); 
  val *= 256; // this is equivalent to val << 8; 

  // send the required ACK 
  pinMode(dataPin, OUTPUT); 
  digitalWrite(dataPin, HIGH); 
  digitalWrite(dataPin, LOW); 
  digitalWrite(clockPin, HIGH); 
  digitalWrite(clockPin, LOW); 

  // get the LSB (less significant bits) 
  pinMode(dataPin, INPUT); 
  val |= shiftIn(dataPin, clockPin, 8); 
  return val; 
} 

// skip CRC data from the SHTx sensor 
void skipCrcSHT(int dataPin, int clockPin) { 
  pinMode(dataPin, OUTPUT); 
  pinMode(clockPin, OUTPUT); 
  digitalWrite(dataPin, HIGH); 
  digitalWrite(clockPin, HIGH); 
  digitalWrite(clockPin, LOW); 
} 
//-------------------------------------------------------------------------------------------

When you run the sketch, it should start off by printing tF followed by the temperature in fahrenheit. After ten seconds, it should display rH folowed by the current relative humidity. After ten more seconds, the cycle will repeat.

alt text

Check out the Product Showcase video to see the dispaly in action.