Assembly Guide for SparkFun JetBot AI Kit V2.0

≡ Pages
Contributors: Evan_Double_U

2. Camera Assembly & Installation

Next, locate the camera mount assembly in the JetBot Chassis Kit. The unassembled view of the parts is laid out in the proper orientation for assembly. The latest revision of the Jetbot Kit includes a camera mount that provides the ability to use stereo vision available on the Jetson Nano Dev Kit V3.

Note: This orientation is necessary to ensure the camera mount fits on the top plate of the chassis.

Unassembled camera mount hardware

Unassembled stereo camera mount hardware

Stereo Camera mount offers 2x camera mount options - left & right

Unpackage the Leopard Imaging camera and assemble the camera mount as shown in the following photograph.

Fully assembled camera mount

Fully assembled stereo camera mount

Having trouble seeing the image? Click on it for a larger view.

Please reference the note about the "Front" of the JetBot in the end of the Introduction to ensure that you mount the camera on the correct side of the camera mount. Align the four holes in the camera mounting plate with those on the camera. Place all four nylon flathead screws through the camera & camera mounting plate prior to fully tightening the nylon nuts. This will ensure equal alignment across all four screws. While holding the nuts in place with a finger, tighten the screws in a rotating criss cross pattern; similar to how you tighten lug nuts on a car rim.

Note: Make sure to orient the camera so the ribbon cable is extending over the "top" of the camera mount as shown below.

camera attached to mount

stereo camera attached to mount

Attach the camera mount & camera to the JetBot Chassis Kit top plate (the unused base plate) using the slightly longer sets of screws and nuts included in the chassis kit (pictured below). Align the plastic tabs on the camera mount to the rectangular cutouts on the front of the chassis top plate. This will result in a sung press fit.

Camera mount fit into the rectangular cutouts on chassis base plate

Stereo Camera mount fit into the rectangular cutouts on chassis base plate

Use the screws to align the holes in the camera assembly with the corresponding holes in the chassis top plate.

Screws inserted into camera mount assembly

Use your small Phillips head screwdriver to thread the screws through the mounting plates. The chassis kit I got was pretty sung and required me to screw them through.

Camera mount screws screwed into chassis

alt text
The Stereo Camera mounts exactly the same to the base plate with a slightly wider footprint

Flip the chassis over & thread two nuts onto the exposed threads of the camera mount hardware.

Nut threaded to camera mount screw

The final assembly will look something like what is pictured below. We have found that this assembly is attached sufficiently by using 2 of 4 screws, but do whatever feels right.

camera mount attached to top plate

alt text
The Stereo Camera mounts exactly the same to the base plate with a slightly wider footprint