Ardumoto Kit Hookup Guide

≡ Pages
Contributors: jimblom, MTaylor

Example Code

Controlling the Ardumoto Shield is super easy. If you can blink LEDs, you can make the Ardumoto Shield spin its motors. Here, we'll provide a simple, expandable example sketch to show how to drive the pair of motors on the Ardumoto.

Note: This example assumes you are using the latest version of the Arduino IDE on your desktop. If this is your first time using Arduino, please read our tutorial on installing Arduino IDE. If you have not previously installed an Arduino library, please check out our installation guide.

The Example Sketch

Download the example sketch and upload it to your board.

language:c
    /* Ardumoto Example Sketch
  by: Jim Lindblom
  date: November 8, 2013
  license: Public domain. Please use, reuse, and modify this 
  sketch!

  Adapted to v20 hardware by: Marshall Taylor
  date: March 31, 2017

  Three useful functions are defined:
    setupArdumoto() -- Setup the Ardumoto Shield pins
    driveArdumoto([motor], [direction], [speed]) -- Drive [motor] 
      (0 for A, 1 for B) in [direction] (0 or 1) at a [speed]
      between 0 and 255. It will spin until told to stop.
    stopArdumoto([motor]) -- Stop driving [motor] (0 or 1).

  setupArdumoto() is called in the setup().
  The loop() demonstrates use of the motor driving functions.
*/

// Clockwise and counter-clockwise definitions.
// Depending on how you wired your motors, you may need to swap.
#define FORWARD  0
#define REVERSE 1

// Motor definitions to make life easier:
#define MOTOR_A 0
#define MOTOR_B 1

// Pin Assignments //
//Default pins:
#define DIRA 2 // Direction control for motor A
#define PWMA 3  // PWM control (speed) for motor A
#define DIRB 4 // Direction control for motor B
#define PWMB 11 // PWM control (speed) for motor B

////Alternate pins:
//#define DIRA 8 // Direction control for motor A
//#define PWMA 9 // PWM control (speed) for motor A
//#define DIRB 7 // Direction control for motor B
//#define PWMB 10 // PWM control (speed) for motor B


void setup()
{
  setupArdumoto(); // Set all pins as outputs
}

void loop()
{
  // Drive motor A (and only motor A) at various speeds, then stop.
  driveArdumoto(MOTOR_A, REVERSE, 255); // Set motor A to REVERSE at max
  delay(1000);  // Motor A will spin as set for 1 second
  driveArdumoto(MOTOR_A, FORWARD, 127);  // Set motor A to FORWARD at half
  delay(1000);  // Motor A will keep trucking for 1 second 
  stopArdumoto(MOTOR_A);  // STOP motor A 

  // Drive motor B (and only motor B) at various speeds, then stop.
  driveArdumoto(MOTOR_B, REVERSE, 255); // Set motor B to REVERSE at max
  delay(1000);  // Motor B will spin as set for 1 second
  driveArdumoto(MOTOR_B, FORWARD, 127);  // Set motor B to FORWARD at half
  delay(1000);  // Motor B will keep trucking for 1 second
  stopArdumoto(MOTOR_B);  // STOP motor B 

  // Drive both
  driveArdumoto(MOTOR_A, FORWARD, 255);  // Motor A at max speed.
  driveArdumoto(MOTOR_B, FORWARD, 255);  // Motor B at max speed.
  delay(1000);  // Drive forward for a second
  // Now go backwards at half that speed:
  driveArdumoto(MOTOR_A, REVERSE, 127);  // Motor A at max speed.
  driveArdumoto(MOTOR_B, REVERSE, 127);  // Motor B at max speed.
  delay(1000);  // Drive forward for a second

  // Now spin in place!
  driveArdumoto(MOTOR_A, FORWARD, 255);  // Motor A at max speed.
  driveArdumoto(MOTOR_B, REVERSE, 255);  // Motor B at max speed.
  delay(2000);  // Drive forward for a second
  stopArdumoto(MOTOR_A);  // STOP motor A 
  stopArdumoto(MOTOR_B);  // STOP motor B 

}

// driveArdumoto drives 'motor' in 'dir' direction at 'spd' speed
void driveArdumoto(byte motor, byte dir, byte spd)
{
  if (motor == MOTOR_A)
  {
    digitalWrite(DIRA, dir);
    analogWrite(PWMA, spd);
  }
  else if (motor == MOTOR_B)
  {
    digitalWrite(DIRB, dir);
    analogWrite(PWMB, spd);
  }  
}

// stopArdumoto makes a motor stop
void stopArdumoto(byte motor)
{
  driveArdumoto(motor, 0, 0);
}

// setupArdumoto initialize all pins
void setupArdumoto()
{
  // All pins should be setup as outputs:
  pinMode(PWMA, OUTPUT);
  pinMode(PWMB, OUTPUT);
  pinMode(DIRA, OUTPUT);
  pinMode(DIRB, OUTPUT);

  // Initialize all pins as low:
  digitalWrite(PWMA, LOW);
  digitalWrite(PWMB, LOW);
  digitalWrite(DIRA, LOW);
  digitalWrite(DIRB, LOW);
}

Then upload to your Arduino and watch your motors spin! If you want to dig really deep into the sketch, check out the comments.

Explaining the Sketch

For each motor there are two mechanisms we can control --- the direction of rotation and the speed. Each of those mechanisms is controlled by one pin on the Arduino.

Controlling Rotation Direction

We can only spin the motor in two directions --- clockwise or counterclockwise --- so we only need two values --- 0 or 1 --- to control that from the Arduino. We can simply digitalWrite either of the direction pins (pin 12 for motor A, pin 13 for motor B) HIGH or LOW to go forward or backward.

For example, if you want motor A to spin clockwise, you simply need to digitalWrite pin 12 LOW:

language:c
digitalWrite(12, LOW);  // Motor A will spin clockwise

To make it spin the other way, write the pin HIGH.

language:c
digitalWrite(12, HIGH);  // Motor A will spin counter-clockwise

(Note: The rotation direction depends on how you wired the motor to your shield. If you swapped the red and black wires, the motor will spin opposite of how we've described it here.)

Speeding

To control the speed of a motor we need to analogWrite to the PWM pins (pin 3 for motor A, pin 11 for motor B). A higher analogWrite value means a faster spin. Writing the pin LOW (or 0) will stop the motor.

PWM ValueMotor Spin Speed
0Off (Stop)
127Half Speed
255Full Speed


If we want to turn motor A up to maximum speed, this is all we need:

language:c
analogWrite(3, 255);  // Motor A at max speed

After that line of code is executed, the motor will spin until stopped. To stop the motor, replace 255 with 0:

language:c
analogWrite(3, 0);  // Stop motor A

Don't forget to set your direction before spinning your motor!