Analog MEMS Microphone Breakout - SPH8878LR5H-1 Hookup Guide

≡ Pages
Contributors: El Duderino, jenfoxbot

Resources and Going Further

Now that you've connected your MEMS microphone breakout, it's time to incorporate it into your own project! For more information on the board, check out the resources below:

If you run into trouble getting, or understanding, an audio signal output from the MEMS mic breakout board, try using a multimeter and/or an oscilloscope to measure the voltage output of the signal in quiet and loud settings. If you're still stuck, check out our forums and we'll help you troubleshoot.

After you've read in the MEMS microphone and have a good handle on the signal output, you're ready to start using it for practical microphone applications! Here are a few ideas to get you started:

  1. Build a music visualizer! Here's a sample sketch for the music visualizer shown in the SparkFun Simple Sketches example.

  2. Record sounds and play them back! You'll also need a speaker, an amplifier transistor, some pushbuttons, and some code. Here's an open-source mbed example. (The example was initially written for the ADMP401 but should work just fine with the latest release).
  3. Make a sound-reactive EL Wire costume and replace the Sound Detector with the MEMS Microphone!
  4. Make a Bark Back Pet Monitor with a Raspberry Pi to record the sound levels in your home, upload the data MQTT, and trigger an audio player to when the volume reaches a threshold.

Or check out these other audio related tutorials below.

Spectacle Audio Board Hookup Guide

All the information you need to use the Spectacle Audio Board in one place.

AzureWave Thing Plus (AW-CU488) Hookup Guide

The SparkFun AzureWave Thing Plus is a Feather form-factor development board equipped with the AW-CU488. We'll highlight key features of the board and show you to get started with the development board. A few Arduino examples will be highlighted to connect to a WiFi router, calculate the Fast Fourier Transform (FFT) from an input microphone, output an analog signal to a speaker, and connect an Qwiic-enabled device.

Qwiic Speaker Amp (TPA2016D2) Hookup Guide

The SparkFun Qwiic Speaker Amp includes the Texas Instruments TPA2016D2 stereo, filter-free class-D audio power amplifier. This tutorial will help you get started and configure the amplifer settings using an Arduino microcontroller.

Audio Codec Breakout - WM8960 Hookup Guide

The SparkFun Audio Codec Breakout - WM8960 is a low power, high quality stereo codec chock full of features. In this tutorial, some of these features by using an Arduino microcontroller to configure the audio codec and pass audio to the headphone or speaker channels.