Analog MEMS Microphone Breakout - SPH8878LR5H-1 Hookup Guide

≡ Pages
Contributors: El Duderino, jenfoxbot

Hardware Assembly

Now that we're familiar with the microphone breakout, let's connect it to a microcontroller and monitor some sound!

Microphone Breakout Connections

For a permanent connection, we recommend soldering three wires (or headers) to the PTHs on the breakout. We opted for soldering wires to the PTH connectors for a quick permanent connection to the breakout. For a temporary connection during prototyping, you can use IC hooks like these.

We recommend using the following colors of wire to easily distinguish the signals but you can always select a different color if you prefer (or do not have the colors used available).

  • Red for VCC
  • Black for GND
  • Yellow (or some other color not Red or Black) for AUD

Wires soldered to MEMS Microphone Breakout

Connecting to a Microcontroller

Next up we'll connect the breakout to a microcontroller we can use to monitor the audio signal output. For this tutorial, we used a SparkFun RedBoard Qwiic. Make the following connections between the breakout and RedBoard Qwiic (or whichever microcontroller you choose):

RedBoard/Arduino MEMS Microphone
A0 AUD
GND GND
3.3V VCC



The completed circuit should look something like the photo below:

Completed MEMS Microphone Breakout Circuit with RedBoard

Read on to the next section for Arduino example code to monitor sound volume with the microphone breakout.