TFMini - Micro LiDAR Module (Qwiic) Hookup Guide

≡ Pages
Contributors: bboyho

Hardware Overview

The sensor works by sending a modulated near-infrared light out. The light that is reflected from the object returns to the sensor's receiver. The distance between the two can be converted using the sensor by calculating the time and phase difference. The distance measured may vary depending on the environment and the reflectivity of object.

Input Power

According to the datasheet (pg 1), the input voltage is 5V. In this tutorial, we will be using the included boost converter by applying a 3.3V input voltage from the Qwiic side to boost power to 5V on the TFMini side.

Benewake TFMini Boost Converter

Logic Levels

While the sensor can be powered at 5V, the I2C pins are only 3.3V logic. Make sure to use a logic level converter when reading the sensor with a 5V microcontroller.

Pinout

There is a marking next to the polarized connector to indicate the polarity as "J1" as indicated in the image below. This is useful when referencing sensor's pinout. As opposed to the original TFMini, the green and white wires for the Qwiic enabled TFMini uses an I2C serial. The default address of the TFMini is 0x10.

TFMini Pinout

Pin Number Wire Color Qwiic TFMini Pinout Wire Color
1 Green SCL (3.3V TTL) Yellow
2 White SDA (3.3V TTL) Blue
3 Red 5V Red
4 Black GND Black