SSOP-16 to DIP Adapter Hookup Guide

≡ Pages
Contributors: Byron J.

Using The Adapter

Adapter Orientation

The pins of the DIP footprint are rotated 90° in relation to the pins of the SSOP. We covered the pin-1 markings for the SSOP in the assembly section.

Pin 1 of the DIP footprint is marked two ways. The solder pad for pin 1 is square, while the others are round. It also has a small 1 in the silkscreen near the pad.

alt text

Pin markings, top

Pins 1 and 9 are also marked in the legend silkscreened on the bottom of the board.

alt text

Pin markings, bottom

Case Studies

On a Breadboard

This adapter is useful when you want to build a breadboard prototype using a chip that's only available in SSOP. It allows the chip to properly fit the rows of the breadboard.

alt text

Breadboard Example

Upgrading Old Devices

Another common use of a SSOP-to-DIP adapter is upgrading or modifying existing equipment...or, as in this case, saving your bacon when you've purchased components with the wrong footprint.

We're working on restoring an old SparkFun Function Generator Kit and needed a 74HC04 logic chip. When we ordered it, we didn't read the description carefully enough, and we got a 14-pin SSOP IC. Unfortunately, it needed to fit it into a DIP footprint on the board. Thankfully, we've got an adapter board to help.

alt text

14 pins in a 16-pin adapter.

If you look closely, you'll notice two things in the above photo: first, the IC only has 14 pins on a 16-pin adapter board. Second, it is a wider SSOP package than we've seen in the other examples. Thankfully, the land pattern on the PCB has extra-long pads to accommodate it.

alt text

Installed in socket.

Since the PCB already had a socket, we opted to use flip pins on the adapter. We're fitting a 14-pin chip on a 16-pin adapter, so we opted to keep pin-1 aligned on both pieces. This also means that the chip is two pins short -- we're not using pins 8 and 9 on the adapter, and pins 10 through 16 on the adapter are off by two, connected to IC pins 8 to 14.