Spectacle Motion Board Hookup Guide

≡ Pages
Contributors: SFUptownMaker

The Configuration Utility

Spectacle Motion Board

The Motion Board page in the Utility provides the following options.

Motion Board Actions

There are four actions associated with the Motion Board, all of which should be used with a single trigger pulse type input signal.

Sweep to Position

Toggle position action

This action moves the motor between two positions, one motion on each trigger event.

  • "listen to channel number ..." - This is the channel which triggers the action.
  • "control servo number ..." - The servo to be controlled, numbered from 0-4.
  • "wait ... seconds and move to" - Delay before motion for the first position.
    • slider control - Choose the position for the first motion. The servo starts at 90° on power up and can be rotated to 0° in one direction or to 180° in the other direction. This is equivalent to starting at 12 o'clock and turning to either 9 o'clock or 3 o'clock.
  • "wait ... seconds and move to" - Delay before motion for the second position.
    • slider control - Choose the position for the second motion. The servo starts at 90° and can be rotated to 0° in one direction or to 180° in the other direction. This is equivalent to starting at 12 o'clock and turning to either 9 o'clock or 3 o'clock.
Sweep and Return

Sweep and return action options

This action waits for a moment, moves the servo to a position, then waits for a moment at the new position, then moves back to the first position.

  • "listen to channel number ..." - Which channel controls this action.
  • "control servo number ..." - The servo to be controlled, numbered from 0-4.
  • "wait ... seconds and move to" - Delay before motion for the first position.
    • slider control - Choose the position for the first motion. The servo starts at 90° and can be rotated to 0° in one direction or to 180° in the other direction. This is equivalent to starting at 12 o'clock and turning to either 9 o'clock or 3 o'clock.
  • "wait ... seconds and move to" - Delay before motion for the second position.
    • slider control - Choose the position for the second motion. The servo starts at 90° and can be rotated to 0° in one direction or to 180° in the other direction. This is equivalent to starting at 12 o'clock and turning to either 9 o'clock or 3 o'clock.
Wagging Effect

Wagging action

This action behaves much like sweep and return, but runs continuously until turned off by receipt of another signal pulse on the designated channel.

  • "listen to channel number ..." - Which channel controls this action.
  • "control servo number ..." - The servo to be controlled, numbered from 0-4.
  • "wait ... seconds and move to" - Delay before motion for the first position.
    • slider control - Choose the position for the first motion. The servo starts at 90° and can be rotated to 0° in one direction or to 180° in the other direction. This is equivalent to starting at 12 o'clock and turning to either 9 o'clock or 3 o'clock.
  • "wait ... seconds and move to" - Delay before motion for the second position.
    • slider control - Choose the position for the second motion. The servo starts at 90° and can be rotated to 0° in one direction or to 180° in the other direction. This is equivalent to starting at 12 o'clock and turning to either 9 o'clock or 3 o'clock.
Go to Position

Go to position options

Move the servo motor from where ever it currently is to this new location after some delay.

  • "listen to channel number ..." - Which channel controls this action.
  • "control servo number ..." - The servo to be controlled, numbered from 0-4.
  • "wait ... seconds and move to" - Delay before motion for the first position.
    • slider control - Choose the position for the first motion. The servo starts at 90° and can be rotated to 0° in one direction or to 180° in the other direction. This is equivalent to starting at 12 o'clock and turning to either 9 o'clock or 3 o'clock.