Spectacle Inertia Board Hookup Guide

≡ Pages
Contributors: SFUptownMaker

Example Project

Let's make a simple project using the Spectacle Audio Board and the Spectacle Inertia Board! We'll set it up so that a sound is played whenever the Inertia Board is moved.

Connect the boards

To follow this tutorial, you'll need this hardware:

Hamburger Mini Speaker

COM-14023
$7.95

Wall Adapter Power Supply - 5.1V DC 2.5A (USB Micro-B)

TOL-13831
$13.95

Spectacle Director Board

DEV-13912
Retired

Spectacle Inertia Board

DEV-13992
Retired

Spectacle Audio Board

DEV-14034
Retired

microSD USB Reader

COM-13004
Retired

Audio Cable TRRS - 3ft

CAB-14164
Retired

microSD Card with Adapter - 16GB (Class 10)

COM-13833
Retired

Note that you will need three of the TRRS cables!

First, plug one end of one of the TRRS cables into the "Direct" jack on the Director Board.

The direct jack

Next, take the other TRRS cable and plug it into the "Program" jack on the Director Board.

The program jack

Take the other end of this cable and plug it into the audio jack of the phone, tablet, or computer that you'll be using to program the system.

Into the phone jack

Plug the other end of that cable into the "In" jack on your Audio Board.

Plugging into the in jack on the audio board

Plug the speaker into the Audio Out port on the Audio Board.

Plugging in the speaker

Take another one of the TRRS cables and plug one end into the "Out" port on the Audio Board...

Plugging into the out jack on the audio board

...and plug the other end of that cable into the "In" port on the Inertia Board.

Plug the other end into the inertia board

Finally, plug the Micro B end of the power adapter into the Director Board and the other end of the adapter into the wall. You should see one solid light and one blinking light on the Inertia Board and the Audio Board. On the Director Board, you'll see one solid light and one light which blinks one time, then pauses, then repeats. This shows that power is present and the boards are up and running.

Setting up the board configuration

When you first visit the Spectacle configuration website, you'll be presented with a screen that looks like this. Your project name will differ, however, as Spectacle assigns a new name to each project. To continue, we're going to have to add our Audio Board to the project.

Blank project

Click on the "Add a Board" button, as highlighted above, to bring up a list of available boards.

Add a board button

In the list, click anywhere in the "Audio" box to add an Audio Board to our project.

Board list

You'll be returned to the main project page, but this time, an Audio Board will appear in the list on the page. Repeat these two steps to add an Inertia Board to the project.

Main page with audio board

Here you can see both boards in the list in place. Next we'll need to add actions to the boards.

List with both boards in place

You can see highlighted above the clapboard icons which, when clicked, will take you to the "Actions" page, where you can assign an action to your board. Let's start by assigning an action to the Audio Board.

Add actions buttons

An empty page will come up. There are no currently assigned actions, so we'll need to assign some. Click the "Add an Action" button at the bottom of the page.

Empty actions page

As you can see, the Audio Board only has one action. Click on "Play Sound" to add this action to your Audio Board.

There's only one action for the sound board

Here are the various settings for the "Play Sound" action. Copy the settings as I've entered them into you project.

Settings for play sound

Click on the "Go Back" button at the bottom of the page to return to the main page, then click on the clapboard icon for the Inertia Board to add an action. When the empty list pops up, click the "Add an Action" button at the bottom to bring up the list of actions for the Inertia Board.

The Go Back button

Here's the list of actions for the Inertia Board. We want to detect when motion occurs, so click the first option, "Sense All Motion".

Inertia board actions

Here's the options page for the sense motion action. Note the choices I've made and duplicate them for your project, then click "Go Back".

Sense motion options

Congratulations! Your project is completed. Now let's upload it to the Director Board.

Project done

Installing a project on the Director Board

Now that you've created your Spectacle program it's time to upload it to the Director Board. If you followed the instructions above, your uploading device is connected to the board and ready to go, so all you need to do is touch the "Install Script" button at the bottom of the page. That will bring up the page seen below.

Upload page

Make sure the volume on your device is turned all the way up, and that no other audio source (music, video, etc) is playing in the background. Then press and hold the "RST" button on the Director Board, press and hold the "PROG" button, then release the "RST" button.

This will put the Director Board into program mode. You'll see the light on the board blink three times, pause, then repeat. This is your visual indicator that the board is in program mode. Once you've established that the board is in program mode, you can begin programming by touching the "Install" button on the Spectacle app screen. The button will gray out during the programming process, which should only last for a few seconds. Once programming is done, you'll see the light on the Director Board blink 10 times, pause, then repeat. That's your cue that the program was uploaded successfully.

Press the "RST" button again to reset the system and begin the program!

If you have any troubles, visit the troubleshooting page for help resolving your issues.