SparkFun SAMD21 Pro RF Hookup Guide

≡ Pages
Contributors: Elias The Sparkiest

Drivers (If You Need Them)

Windows 10

After plugging the board in, Windows will try to search the Internet for drivers. They should automatically install for Windows 10 without any issues.

Windows 7

If you are using a Windows 7 OS, you will need to install the SAMD drivers using the SAMD Windows 7 Installer. Head over to the GitHub repo to install the executable.

Scroll down the page to the assets in the Latest release and click on the '.exe to download. The version number may be different depending on the release. The image below shows sparkfun_drivers_1.0.5.3.exe .

Windows 7 Driver Download

Click on the image for a closer view.

After downloading, click on the executable and follow the prompts to install. The steps to install are the same even though the following images show drivers for v1.0.5.1.

SparkFun Driver Executable

You will receive a warning from Windows. Click yes to continue.

Windows 7 Warning

Another window will pop up. Read through the license and click "I Agree".

License Agreement

When ready, hit the Install button.

Install SAMD Drivers

Another window will pop up. Click on "Install this driver software anyway" to continue.

Windows Warning

Your Windows 7 will begin installing the driver. This should take a few seconds. When the drivers have installed, hit the "Close" button to exit out of the installer.

Successful Install

Mac and Linux

Mac and Linux users shouldn't need to download any drivers. The device should show up as a serial port as soon as it's plugged in to your computer.