Comments: SparkFun RFID Starter Kit Hookup Guide

≡ Pages

Looking for answers to technical questions?

We welcome your comments and suggestions below. However, if you are looking for solutions to technical questions please see our Technical Assistance page.

  • Member #1800059 / about 4 years ago / 1

    I'm using Arduino IDE, ID-20LA and compatible tags from sparkfun. When I scan the tags im getting empty boxes before and sometimes after the tag number. How do I stop this?

  • Member #1502072 / about 8 years ago / 1

    How do i use this without arduino?

  • Member #628385 / about 8 years ago / 1

    Is there any way to disable the beeping sound?

  • Member #1369744 / about 8 years ago / 1

    Using Node.js to read from the reading using node-serialport. Getting reading coming in but my numbers don't match what is on the card. I assume this is something to do with encoding but I'm not sure. Anyone able to help me? I scan a card with the printed numbers "0000818960" and I get "0A000C7F1069" when I do "data.toString('ascii')" on the data coming from node-serial port. Thoughts?

  • -------------------- Tech Support Tips/Troubleshooting/Common Issues --------------------

    Read Ranges Using the RFID USB Reader

    Using the ID Innovations125kHz readers, the tested real world maximum ranges of the modules with the RFID tagged items are listed below:

    ID-3LA

    Card = 0" (you need an external antenna)
    Button = 0" (you need an external antenna)
    Glass Capsule = 0" (you need an external antenna)
    

    ID12-LA

    Card = 2" - 2.25"
    Button = 1" - 1.5"
    Glass Capsule = 0.75" - 1"
    

    ID20-LA

    Card = 2.75"
    Button = 2"
    Glass Capsule = 0.75"
    

    The range results were taken from the demo video between 6:13-9:10 => https://youtu.be/FLjV5BT9slg?t=6m13s .

    Multiple RFID USB Readers

    If you place 4 of these RFID readers with the ID Readers, there will be RF interference from each other. Customer had issues with this setup. When he placed them at a distance of about 15-20cm+ between each other, they were able to get them working.

  • Member #828081 / about 10 years ago / 1

    I've been having issues with my RFID. I'm not sure if it's in the wiring, the code, or just a bad component, but I was hoping for some advice.

    I've used your code, as well as 4 others that I found on google, each of which returned the serial values "255 255 255 255...", so I kind of doubt its the code. (I should mention I put in a Serial.print(readByte) in the loop to see what the integer values were)

    It is hooked up as follows:

    Arduino ID-20 5V VCC GND GND D2 D0

    Lastly, I assume the components work fine, because it never returns any serial values to my com port until I wave the tag in front of it.

    Any ideas?

  • Member #790185 / about 11 years ago / 1

    The code example does not work correctly.

    total = checkTag(newTag, knownTags[ct]);

    should be

    total += checkTag(newTag, knownTags[ct]);

    Otherwise only the last card in the array will ever work. Cheers CJ

  • Member #775731 / about 11 years ago / 1

    do i need to use arduino with RFID reader starter kit to save tags ID ?

    • a_cavis / about 11 years ago / 2

      You don't have to use an Arduino, but you do need something on the other end to capture and save the data. You could do it with a PC over USB, or use the serial output or the USB output with a Raspberry Pi or another single-board computer.


If you've found an issue with this tutorial content, please send us your feedback!