SparkFun Qwiic Button Hookup Guide
Contributors:
El Duderino
Resources and Going Further
For more information, check out the resources below:
- Schematic (PDF)
- Eagle Files (ZIP)
- Board Dimensions (PNG)
- Qwiic Button Arduino Library
- Qwiic Button Python Package
- GitHub Hardware Repo
- SFE Product Showcase
Need help getting started with Arduino and I2C? Check out these resources:
- Arduino I2C Scanner Example
- Arduino Wire Library Reference Page
- Arduino Wire Library (In-Depth) Reference
Looking for some inspiration for a project using the Qwiic Button? Check out this GPS Geo-Mapping project by Brandon J. Williams.
Before you go, here are some other tutorials using the Qwiic Connect System you may want to look through:
ESP32 LoRa 1-CH Gateway, LoRaWAN, and the Things Network
Using the ESP32 LoRa 1-CH Gateway as a gateway and device, and pushing data to The Things Network.
TFMini - Micro LiDAR Module (Qwiic) Hookup Guide
The TFMini is a ToF (Time of Flight) LiDAR sensor capable of measuring the distance to an object as close as 30 cm and as far as 12 meters! The TFMini allows you to easily integrate LiDAR into applications traditionally reserved for smaller sensors such as the SHARP GP-series infrared rangefinders. With the added Qwiic feature, you can quickly connect to the sensor via I2C!
SparkFun Qwiic Shield for Arduino Nano Hookup Guide
Hookup Guide for the SparkFun Qwiic Shield for Arduino Nano.
MicroMod Asset Tracker Carrier Board Hookup Guide
Get started with the SparkFun MicroMod Asset Tracker Carrier Board following this Hookup Guide. The Asset Tracker uses the u-blox SARA-R510M8S LTE-M / NB-IoT module to provide a host of data communication options.