SparkFun Air Quality Sensor - SGP30 (Qwiic) Hookup Guide

≡ Pages
Contributors: El Duderino, Englandsaurus

Hardware Assembly

Using the Qwiic system, assembling the hardware is a breeze. All you need to do is connect your SparkFun Air Quality Sensor - SGP30 (Qwiic) to your chosen development board with a Qwiic cable or adapter cable. If you would prefer to not use the Qwiic connectors, you can connect to the 0.1" header pins broken out on bottom of the board.

Air Quality Sensor connected to a RedBoard Qwiic

If you decide to use the PTH pins broken out on the Air Quality Sensor you will need to solder to them. Alternatively, if you want a temporary connection for prototyping, these IC Hooks are a great option to make that connection. If you are not familiar with through-hole soldering take a look at this tutorial:

How to Solder: Through-Hole Soldering

September 19, 2013
This tutorial covers everything you need to know about through-hole soldering.

With the SGP30 connected to your microcontroller it's time to get some code uploaded and start taking measurements!