Sound Reactive EL Wire Costume

≡ Pages
Contributors: jenfoxbot

Build It!

CAUTION: Although it is low current, EL wire runs on high voltage AC (100 VAC). There are exposed connections on the EL Sequencer board so BE CAREFUL when handling the board. Always double (and triple) check that the power switch is OFF before touching any part of the board. For final projects, it is recommended to coat all exposed connections in epoxy, hot glue, electrical tape, or other insulating material.
  1. Test EL Sequencer with EL Wire.

    alt text

    Connect the inverter, battery, and at least one strand of EL wire to the EL Sequencer. (Note that the two black wires of the inverter correspond to the AC side.)

    Be sure that the EL Wire lights up and blinks when you power the EL Sequencer on battery mode.

  2. Solder header pins onto 5V FTDI pinholes on the EL Sequencer and onto the VCC, Ground, and A2 input pins.

    alt text

  3. Solder header pins to the sound detector.

    alt text

  4. Connect sound detector to EL Sequencer via female-to-female jumper wires (you can also skip the header installation, and solder wire directly to the header pins).

    alt text

    Connect the sound detector VCC and Ground pins to the VCC and Ground pins on the EL Sequencer. Connect the sound detector Gate output to the A2 input pin on the EL Sequencer. If you are using the envelope and/or audio output signals, connect these to pins A3 and A4 on the EL Sequencer (more on this in the Program It! section below).

  5. Make a protective casing for the sound detector using packing foam or styrofoam to prevent jostling or other physical vibrations (aka collisions) from triggering it.

    alt text

    alt text

    Place sound detector on top of foam, outline the board with a pen, and cut out a hole in the foam for the detector to fit snugly inside. It is also recommended that you epoxy the wires onto the foam (but not the sound detector board).

  6. Cut out a pocket from the jacket, and sew onto the belt.

    alt text

    alt text

  7. Put belt on, connect EL Wire to EL Sequencer, and place EL Sequencer in pocket pouch. Determine approximate placement of each EL wire strand based on location of electronics.

    alt text

  8. Mark and/or adhere the base of the EL wire JST connector onto clothing, allowing the full length of the connector to flex. Be sure that the JST connector can easily reach the EL Sequencer.

    alt text

  9. Starting at the base of the JST connector, attach EL wire strands to your chosen article of clothing.

    alt text

    Sew EL wire onto clothing using strong thread or dental floss, or use an appropriate fabric adhesive.

    alt text

    Prior to adhering the EL wire, it is recommended to use safety pins to determine placement of the EL wire on each article of clothing while you are wearing it. EL wire is flexible but not so stretchy, so give yourself some wiggle room.

    It is also recommended to use separate EL wire strands on different articles of clothing to facilitate the process of taking it on/off.