Sensor System Hookup Guide

≡ Pages
Contributors: MikeGrusin

Recording Data with the Sensor System

1. Insert the MicroSD Card into the Sensor System

With the Sensor System unplugged from any power supplies, gently insert the microSD card into the slot on the right side of the front panel. It will only fit one way; the gold pads on the microSD card should be facing down and the label should be facing up.

Inserting a microSD Card to the Sensor System

Note that this microSD socket does not "click" like some sockets do. Simply press the card into the slot until it stops. A portion of the microSD card will protrude from the panel, allowing you to remove it later.

Lost card? It's easy for the microSD card to slip past the socket and rattle around inside the Sensor System. If this happens, disassemble the Sensor System by removing the screws on the underside of the box, and retrieve the lost card.

3. Plug the USB Power Cable into the Sensor System

The Sensor System runs on USB power. This could come from a Wall Adapter, or a USB Battery Pack for portable use.

Plug the micro-B USB end of the cable into the Sensor System. This connector has a subtle "D" shape to it, and will only fit one way. It should snap securely into the Sensor System.

Powering the Sensor System

Now plug the other end of the USB Cable into your USB power supply if it isn't already.

Note: The USB cable is only used to power the Sensor System. It is not used to transfer data.

4. Turn On the Sensor System

Briefly press the power button on the left side of the Sensor System's front panel. The STAT LED will blink once or twice, then light up solid red if everything is plugged in correctly.

Power Up the Sensor Systemk

If the LED keeps blinking, the number of blinks can help you find the problem. See the Troubleshooting section below.

5. Begin Recording Data

When your Sensor System is in the location you want to study and you're ready to begin recording, briefly press the USR button on the front panel of the Sensor System. The LED will turn green and flash each time it records new data.

Start Logging Data with the Sensor System

Note: When you're done recording data, be sure to follow the next two steps before removing the microSD card. Failure to do so could result in corrupted data or an unreadable card.

6. Stop Recording Data

When you're finished recording data, briefly press the USR button on the front panel of the Sensor System. The LED will turn red to indicate that recording has stopped.

Stopping Recording with the Sensor System

7. Turn Off the Sensor System

Briefly press the power button on the left side of the front panel of the Sensor System. The LED will turn off.

Power Down the Sensor System

8. Remove the MicroSD Card

Once the Sensor System is turned off, grip the protruding end of the microSD card and gently pull it out of the Sensor System. You can now insert the microSD card into an adapter (USB reader or full-size SD card) and read the data using your computer.