RETIRED (Phant Examples) - ESP8266 Thing Development Board Hookup Guide

This Tutorial is Retired!

This tutorial covers concepts or technologies that are no longer current. It's still here for you to read and enjoy, but may not be as useful as our newest tutorials.

≡ Pages
Contributors: jimblom

Introduction

Phant is No Longer in Operation

Unfortunately Phant, our data-streaming service, is no longer in service. The system has reached capacity and, like a less-adventurous Cassini, has plunged conclusively into a fiery and permanent retirement. There are several other maker-friendly, data-streaming services and/or IoT platforms available as alternatives. The three we recommend are Blynk, ThingSpeak, and Cayenne. You can read our blog post on the topic for an overview and helpful links for each platform. The code in this tutorial will need to be adjusted to work with the other data streams.

An archived tutorial of our first ESP8266 Thing development board example used in our ESP8266 Thing Development Board Hookup Guide. This example showed you how you can use the Thing Dev Board to post data to data.sparkfun.com.

Suggested Reading

Before continuing on with this tutorial, you may want to familiarize yourself with some of these topics if they’re unfamiliar to you:

ESP8266 Thing Development Board Hookup Guide

November 5, 2015
An overview of SparkFun's ESP8266 Thing Development Board - a development board for the Internet of Things.

Example Sketch: Posting to Phant

When we develop Internet-enabled development platforms, our version of "Hello, world" is posting to data.sparkfun.com -- our free online data storage service running our open-source Phant software.

Here's a simple example sketch that posts four values to a test stream. Feel free to use that stream temporarily to make sure your Thing Dev Board is working (don't abuse it please!).

Install the Phant Library! This example makes use of the SparkFun Phant Arduino library, to make assembling Phant POSTs as easy as possible.

The Phant library can be installed using Arduino's Library Manager. Go to the Sketch > Include Library > Manage Libraries..., then search for "Phant" to find the library. Install the latest version (or at least 2.2.0).



Or you can grab the Phant library from our phant-arduino repository, and follow along with our Installing an Arduino Library for help installing the library.

Copy the code below, or download the example sketch.

Before uploading your code to the Thing, make sure you modify the WiFiSSD and WiFiPSK variables, setting them to the SSID and password of your WiFi network. The rest of the sketch should just work.

language:c
// Include the ESP8266 WiFi library. (Works a lot like the
// Arduino WiFi library.)
#include <ESP8266WiFi.h>
// Include the SparkFun Phant library.
#include <Phant.h>

//////////////////////
// WiFi Definitions //
//////////////////////
const char WiFiSSID[] = "WiFi_Network";
const char WiFiPSK[] = "WiFi_Password";

/////////////////////
// Pin Definitions //
/////////////////////
const int LED_PIN = 5; // Thing's onboard, green LED
const int ANALOG_PIN = A0; // The only analog pin on the Thing
const int DIGITAL_PIN = 12; // Digital pin to be read

////////////////
// Phant Keys //
////////////////
const char PhantHost[] = "data.sparkfun.com";
const char PublicKey[] = "wpvZ9pE1qbFJAjaGd3bn";
const char PrivateKey[] = "wzeB1z0xWNt1YJX27xdg";

/////////////////
// Post Timing //
/////////////////
const unsigned long postRate = 60000;
unsigned long lastPost = 0;

void setup() 
{
  initHardware(); // Setup input/output I/O pins
  connectWiFi(); // Connect to WiFi
  digitalWrite(LED_PIN, LOW); // LED on to indicate connect success
}

void loop() 
{
  // This conditional will execute every lastPost milliseconds
  // (assuming the Phant post succeeded).
  if ((lastPost + postRate <= millis()) || lastPost == 0)
  {
    Serial.println("Posting to Phant!");
    if (postToPhant())
    {
      lastPost = millis();
      Serial.println("Post Suceeded!");
    }
    else // If the Phant post failed
    {
      delay(500); // Short delay, then try again
      Serial.println("Post failed, will try again.");
    }
  }
}

void connectWiFi()
{
  byte ledStatus = LOW;
  Serial.println();
  Serial.println("Connecting to: " + String(WiFiSSID));
  // Set WiFi mode to station (as opposed to AP or AP_STA)
  WiFi.mode(WIFI_STA);

  // WiFI.begin([ssid], [passkey]) initiates a WiFI connection
  // to the stated [ssid], using the [passkey] as a WPA, WPA2,
  // or WEP passphrase.
  WiFi.begin(WiFiSSID, WiFiPSK);

  // Use the WiFi.status() function to check if the ESP8266
  // is connected to a WiFi network.
  while (WiFi.status() != WL_CONNECTED)
  {
    // Blink the LED
    digitalWrite(LED_PIN, ledStatus); // Write LED high/low
    ledStatus = (ledStatus == HIGH) ? LOW : HIGH;

    // Delays allow the ESP8266 to perform critical tasks
    // defined outside of the sketch. These tasks include
    // setting up, and maintaining, a WiFi connection.
    delay(100);
    // Potentially infinite loops are generally dangerous.
    // Add delays -- allowing the processor to perform other
    // tasks -- wherever possible.
  }
  Serial.println("WiFi connected");  
  Serial.println("IP address: ");
  Serial.println(WiFi.localIP());
}

void initHardware()
{
  Serial.begin(9600);
  pinMode(DIGITAL_PIN, INPUT_PULLUP); // Setup an input to read
  pinMode(LED_PIN, OUTPUT); // Set LED as output
  digitalWrite(LED_PIN, HIGH); // LED off
  // Don't need to set ANALOG_PIN as input, 
  // that's all it can be.
}

int postToPhant()
{
  // LED turns on when we enter, it'll go off when we 
  // successfully post.
  digitalWrite(LED_PIN, LOW);

  // Declare an object from the Phant library - phant
  Phant phant(PhantHost, PublicKey, PrivateKey);

  // Do a little work to get a unique-ish name. Append the
  // last two bytes of the MAC (HEX'd) to "Thing-":
  uint8_t mac[WL_MAC_ADDR_LENGTH];
  WiFi.macAddress(mac);
  String macID = String(mac[WL_MAC_ADDR_LENGTH - 2], HEX) +
                 String(mac[WL_MAC_ADDR_LENGTH - 1], HEX);
  macID.toUpperCase();
  String postedID = "ThingDev-" + macID;

  // Add the four field/value pairs defined by our stream:
  phant.add("id", postedID);
  phant.add("analog", analogRead(ANALOG_PIN));
  phant.add("digital", digitalRead(DIGITAL_PIN));
  phant.add("time", millis());

  // Now connect to data.sparkfun.com, and post our data:
  WiFiClient client;
  const int httpPort = 80;
  if (!client.connect(PhantHost, httpPort)) 
  {
    // If we fail to connect, return 0.
    return 0;
  }
  // If we successfully connected, print our Phant post:
  client.print(phant.post());

  // Read all the lines of the reply from server and print them to Serial
  while(client.available()){
    String line = client.readStringUntil('\r');
    //Serial.print(line); // Trying to avoid using serial
  }

  // Before we exit, turn the LED off.
  digitalWrite(LED_PIN, HIGH);

  return 1; // Return success
}

After loading the code onto your Thing, it will begin to run. The status LED connected to pin 5 will initially blink at about 2 Hz. After the Thing connects to your network, the green LED will turn solid and post to the test stream. At that point the LED will go dark, only blinking every 60s-or-so as the Thing posts to Phant again.

If the LED never stops blinking, your Thing is probably having trouble connecting to the WiFi network. Make sure the SSID and PSK variables are set correctly.

Four values are posted to the Phant stream: the reading from the ADC pin, a digital reading from pin 12, the Thing's ID ("Thing" appended with the last two MAC bytes), and a time variable loaded from the millis() function. Load up the test stream to check for your Thing's signature there!

Screenshot of data stream

Example screenshot from our communal data.sparkfun.com stream.

Read through the comments in the code to get a line-by-line breakdown of what's going on in the sketch. Then try creating a stream of your own, see what other data you can log!

Resources and Going Further

Need a little project inspiration for using the ESP8266 in web client mode with a different data-streaming service and/or IoT platform? Check out this tutorial to log data with ThingSpeak.

Internet of Things Experiment Guide

November 23, 2016
The SparkFun ESP8266 Thing Dev Board is a powerful development platform that lets you connect your hardware projects to the Internet. In this guide, we show you how to combine some simple components to remotely log temperature data, send yourself texts and control lights from afar.