RETIRED - SparkFun Inventor's Kit Experiment Guide - v4.0
This Tutorial is Retired!
This tutorial covers concepts or technologies that are no longer current. It's still here for you to read and enjoy, but may not be as useful as our newest tutorials.
View the updated tutorial: SparkFun Inventor's Kit Experiment Guide - v4.0
Install the Arduino IDE and SIK Code
The following steps are a basic overview of getting started with the Arduino IDE. For more detailed, step-by-step instructions for setting up the Arduino IDE on your computer, please check out the following tutorial.
Installing Arduino IDE
Download the Arduino IDE
In order to get your microcontroller up and running, you'll need to download the newest version of the Arduino software first (it's free and open source!).
This software, known as the Arduino IDE, will allow you to program the board to do exactly what you want. It’s like a word processor for writing code.
Download Arduino Code
You are so close to to being done with setup! Download the SIK Guide Code. You can also download the code from GitHub or click the following link to download the code:
Place the SIK-Guide-Code folder in the Arduino IDE examples directory:
- Windows: drag the
SIK-Guide-Codefolder intoC:\Program Files\Arduino-x\examples
- MacOS: Right-click on the Arduino IDE app and click "Show Package Contents...". Drag the
SIK-Guide-Codefolder intoContents/Resources/Java - Linux: see http://www.arduino.cc/playground/Learning/Linux
Connect the Microcontroller to your Computer
Use the USB cable provided in the SIK kit to connect the included microcontroller (RedBoard or Arduino Uno) to one of your computer’s USB inputs.
Install FTDI Drivers
Depending on your computer’s operating system, you will need to follow specific instructions. Please go to How to Install FTDI Drivers, for specific instructions on how to install the FTDI drivers onto your RedBoard.
USB Serial Driver Quick Install
Select your Board: Arduino/Genuino Uno
Before we can start jumping into the experiments, there are a couple adjustments we need to make. This step is required to tell the Arduino IDE which of the many Arduino boards we have. Go up to the Tools menu. Then hover over Board and make sure Arduino Uno is selected.
Select a Serial Port
Next up we need to tell the Arduino IDE which of our computer's serial ports the microcontroller is connected to. For this, again go up to Tools, then hover over Port (Serial Port in older Arduino versions) and select your RedBoard or Arduino's serial port. This will be the same serial port seen when installing FTDI drivers.
With that, you're now ready to begin building your first circuit!