Qwiic Dynamic NFC/RFID Tag Hookup Guide

≡ Pages
Contributors: El Duderino

Introduction

The SparkFun Qwiic Dynamic NFC/RFID Tag features the ST25DV64KC dynamic Near Frequency Communication (NFC) / Radio Frequency Identification (RFID) tag IC from STMicroelectronics©. The ST25DV64KC offers 64-kBit (8-kBytes) of EEPROM memory which can be accessed over both I2C and RF (NFC)! It's a state-of-the-art tag which conforms to ISO/IEC 15693 or NFC Forum Type 5 recommendations. You can read and write the tag's memory using NFC even while the tag is powered down or disconnected!

SparkFun Qwiic Dynamic NFC/RFID Tag

SEN-21274
$11.95

In this guide we'll go into some detail on the ST25DV64KC IC and other hardware on this Qwiic breakout, how to assemble it into a Qwiic circuit and then install the SparkFun ST25DV64KC Arduino Library.

Required Materials

To follow along with this guide you will need a microcontroller to communicate with the Qwiic Dynamic NFC/RFID Tag. Below are a few options that come Qwiic-enabled out of the box:

SparkFun RedBoard Plus

DEV-18158
$29.50

SparkFun Thing Plus - ESP32 WROOM (Micro-B)

WRL-15663
$24.95

SparkFun Thing Plus - Artemis

WRL-15574
$25.95

SparkFun RedBoard Artemis

DEV-15444
$24.95

If your chosen microcontroller is not already Qwiic-enabled, you can add that functionality with one or more of the following items:

SparkFun Qwiic Cable Kit

KIT-15081
$12.95

SparkFun Qwiic Adapter

DEV-14495
$1.60

SparkFun Qwiic Shield for Arduino

DEV-14352
$7.75

SparkFun Qwiic Shield for Thing Plus

DEV-16790
$5.10

You will also need at least one Qwiic cable to connect your sensor to your microcontroller.

Qwiic Cable - 50mm

PRT-14426
Retired

Qwiic Cable - 100mm

PRT-14427
Retired

Qwiic Cable - 200mm

PRT-14428
Retired

Qwiic Cable - 500mm

PRT-14429
Retired

Optional Materials

Suggested Reading

If you aren't familiar with the Qwiic system, we recommend reading here for an overview.

Qwiic Connect System

We also recommend taking a look at the following tutorials if you aren't familiar with the concepts covered in them. If you are using one of the Qwiic Shields listed above, you may want to read through their respective Hookup Guides as well before you get started with the Qwiic Dynamic NFC/RFID Tag.

I2C

An introduction to I2C, one of the main embedded communications protocols in use today.

RFID Basics

Dive into the basics of Radio Frequency Identification (RFID) technology.

Qwiic Shield for Arduino & Photon Hookup Guide

Get started with our Qwiic ecosystem with the Qwiic shield for Arduino or Photon.

SparkFun Qwiic Shield for Arduino Nano Hookup Guide

Hookup Guide for the SparkFun Qwiic Shield for Arduino Nano.