MS5803-14BA Pressure Sensor Hookup Guide
Contributors:
CaseyTheRobot
Resources and Going Further
Now that you've successfully got your MS5803-14BA Pressure Sensor up and running, it's time to incorporate it into your own project! For more information, check out the resources below:
- Schematic
- Eagle Files
- Datasheet (MS5803-14BA)
- GitHub
- SFE Product Showcase
Need some inspiration for your next project? Check out some of these related tutorials:
SparkFun gator:soil Hookup Guide
The gator:soil is analog soil moisture sensor. This tutorial will get you started using the gator:soil with the micro:bit platform.
Artemis Global Tracker Hookup Guide
The SparkFun Artemis Global Tracker combines the Artemis processor with an Iridium 9603N satellite transceiver, ZOE-M8Q GNSS transceiver, and MS8607 PHT sensor. With a clear view of the sky, this board allows you to send and receive short data messages from anywhere in the world including remote locations far beyond the reach of WiFi and GSM networks. Follow this guide to get started with the Artemis Global Tracker.
SparkFun Thing Plus - NINA-B306 Hookup Guide
A quick guide to get started using the SparkFun Thing Plus - NINA-B306. This Thing Plus is loaded with the Arm Cortex-M4 processor in the NINA-B306 along with on-board motion and environmental sensors in the ISM330DHCX 6DoF and BME280 pressure and temperature sensor.
Qwiic Kit for Raspberry Pi V2 Hookup Guide
Get started with the SGP40, BME280, VCNL4040, and microOLED via I2C using the Qwiic system and Python on a Raspberry Pi! Measure VOC Index, light, temperature, humidity, and pressure from the environment. Then display them on the microOLED, serial terminal, or the cloud with Cayenne!
Tip: If you are submerging the sensor in a liquid, try sealing the board in silicone conformal coating while keeping the gel membrane exposed to the medium. Just keep in mind that the antimagnetic stainless steel cap only protects against "30 bar overpressure water resistance" as stated in the datasheet.
If you have any problems or questions, our technical support department can help. Please don't hesitate to contact us. We also love to hear about your projects!